public static class ShelfBuilder.LengthMethods extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FULL |
static int |
_SHELF_FROM_END |
static int |
_STEP_FROM_END |
static int |
_TO_SELECTED |
static ShelfBuilder.LengthMethods |
FULL |
static ShelfBuilder.LengthMethods |
SHELF_FROM_END |
static ShelfBuilder.LengthMethods |
STEP_FROM_END |
static ShelfBuilder.LengthMethods |
TO_SELECTED |
Modifier and Type | Method and Description |
---|---|
static ShelfBuilder.LengthMethods |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShelfBuilder.LengthMethods |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShelfBuilder.LengthMethods[] |
values()
Returns an array that contains the values for this enum.
|
public static final ShelfBuilder.LengthMethods FULL
public static final ShelfBuilder.LengthMethods SHELF_FROM_END
public static final ShelfBuilder.LengthMethods STEP_FROM_END
public static final ShelfBuilder.LengthMethods TO_SELECTED
public static final int _FULL
public static final int _SHELF_FROM_END
public static final int _STEP_FROM_END
public static final int _TO_SELECTED
public static ShelfBuilder.LengthMethods valueOf(int value)
public static ShelfBuilder.LengthMethods valueOf(String name)
public static ShelfBuilder.LengthMethods[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.