public static class SectionSurfaceBuilderEx.CubicType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FILLET_BRIDGE
Fillet Bridge mode
|
static int |
_TWO_SLOPES
Two Slopes mode
|
static SectionSurfaceBuilderEx.CubicType |
FILLET_BRIDGE
Fillet Bridge mode
|
static SectionSurfaceBuilderEx.CubicType |
TWO_SLOPES
Two Slopes mode
|
Modifier and Type | Method and Description |
---|---|
static SectionSurfaceBuilderEx.CubicType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilderEx.CubicType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilderEx.CubicType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SectionSurfaceBuilderEx.CubicType TWO_SLOPES
public static final SectionSurfaceBuilderEx.CubicType FILLET_BRIDGE
public static final int _TWO_SLOPES
public static final int _FILLET_BRIDGE
public static SectionSurfaceBuilderEx.CubicType valueOf(int value)
public static SectionSurfaceBuilderEx.CubicType valueOf(String name)
public static SectionSurfaceBuilderEx.CubicType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.