public static class RPOBuilder.AssociativityType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ARC_CENTER
Arc-center
|
static int |
_END_POINT
End-point (determined from 3d help point)
|
static int |
_END_POINT1
1st end point (at minimum parameter value)
|
static int |
_END_POINT2
2nd end point
|
static int |
_HORIZONTAL_CENTERLINE1
horizontal centerline end point 1
|
static int |
_HORIZONTAL_CENTERLINE2
horizontal centerline end point 2
|
static int |
_TANGENCY
Tangency
|
static int |
_VERTICAL_CENTERLINE1
vertical centerline end point 1
|
static int |
_VERTICAL_CENTERLINE2
vertical centerline end point 2
|
static RPOBuilder.AssociativityType |
ARC_CENTER
Arc-center
|
static RPOBuilder.AssociativityType |
END_POINT
End-point (determined from 3d help point)
|
static RPOBuilder.AssociativityType |
END_POINT1
1st end point (at minimum parameter value)
|
static RPOBuilder.AssociativityType |
END_POINT2
2nd end point
|
static RPOBuilder.AssociativityType |
HORIZONTAL_CENTERLINE1
horizontal centerline end point 1
|
static RPOBuilder.AssociativityType |
HORIZONTAL_CENTERLINE2
horizontal centerline end point 2
|
static RPOBuilder.AssociativityType |
TANGENCY
Tangency
|
static RPOBuilder.AssociativityType |
VERTICAL_CENTERLINE1
vertical centerline end point 1
|
static RPOBuilder.AssociativityType |
VERTICAL_CENTERLINE2
vertical centerline end point 2
|
Modifier and Type | Method and Description |
---|---|
static RPOBuilder.AssociativityType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RPOBuilder.AssociativityType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RPOBuilder.AssociativityType[] |
values()
Returns an array that contains the values for this enum.
|
public static final RPOBuilder.AssociativityType END_POINT
public static final RPOBuilder.AssociativityType ARC_CENTER
public static final RPOBuilder.AssociativityType TANGENCY
public static final RPOBuilder.AssociativityType END_POINT1
public static final RPOBuilder.AssociativityType END_POINT2
public static final RPOBuilder.AssociativityType VERTICAL_CENTERLINE1
public static final RPOBuilder.AssociativityType VERTICAL_CENTERLINE2
public static final RPOBuilder.AssociativityType HORIZONTAL_CENTERLINE1
public static final RPOBuilder.AssociativityType HORIZONTAL_CENTERLINE2
public static final int _END_POINT
public static final int _ARC_CENTER
public static final int _TANGENCY
public static final int _END_POINT1
public static final int _END_POINT2
public static final int _VERTICAL_CENTERLINE1
public static final int _VERTICAL_CENTERLINE2
public static final int _HORIZONTAL_CENTERLINE1
public static final int _HORIZONTAL_CENTERLINE2
public static RPOBuilder.AssociativityType valueOf(int value)
public static RPOBuilder.AssociativityType valueOf(String name)
public static RPOBuilder.AssociativityType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.