public static class PointSetBuilder.PatternLimitsType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DIAGONAL_POINTS
The pattern limit is defined by two points.
|
static int |
_PERCENTAGES
The pattern limit is defined by surface U and V values.
|
static PointSetBuilder.PatternLimitsType |
DIAGONAL_POINTS
The pattern limit is defined by two points.
|
static PointSetBuilder.PatternLimitsType |
PERCENTAGES
The pattern limit is defined by surface U and V values.
|
Modifier and Type | Method and Description |
---|---|
static PointSetBuilder.PatternLimitsType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PointSetBuilder.PatternLimitsType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PointSetBuilder.PatternLimitsType[] |
values()
Returns an array that contains the values for this enum.
|
public static final PointSetBuilder.PatternLimitsType DIAGONAL_POINTS
public static final PointSetBuilder.PatternLimitsType PERCENTAGES
public static final int _DIAGONAL_POINTS
public static final int _PERCENTAGES
public static PointSetBuilder.PatternLimitsType valueOf(int value)
public static PointSetBuilder.PatternLimitsType valueOf(String name)
public static PointSetBuilder.PatternLimitsType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.