public static class MoveFaceBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ROTATE_ABOUT_AXIS
Move faces by rotating about an axis
|
static int |
_ROTATE_BETWEEN_TWO_AXES
Move faces by rotating the axis from the first to the second
|
static int |
_TRANSLATE_BETWEEN_TWO_POINTS
Move faces in the direction and distance defined by the two points
|
static int |
_TRANSLATE_DIRECTION_AND_DISTANCE
Direction and Distance for moving the faces
|
static MoveFaceBuilder.Types |
ROTATE_ABOUT_AXIS
Move faces by rotating about an axis
|
static MoveFaceBuilder.Types |
ROTATE_BETWEEN_TWO_AXES
Move faces by rotating the axis from the first to the second
|
static MoveFaceBuilder.Types |
TRANSLATE_BETWEEN_TWO_POINTS
Move faces in the direction and distance defined by the two points
|
static MoveFaceBuilder.Types |
TRANSLATE_DIRECTION_AND_DISTANCE
Direction and Distance for moving the faces
|
Modifier and Type | Method and Description |
---|---|
static MoveFaceBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MoveFaceBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MoveFaceBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final MoveFaceBuilder.Types TRANSLATE_DIRECTION_AND_DISTANCE
public static final MoveFaceBuilder.Types TRANSLATE_BETWEEN_TWO_POINTS
public static final MoveFaceBuilder.Types ROTATE_ABOUT_AXIS
public static final MoveFaceBuilder.Types ROTATE_BETWEEN_TWO_AXES
public static final int _TRANSLATE_DIRECTION_AND_DISTANCE
public static final int _TRANSLATE_BETWEEN_TWO_POINTS
public static final int _ROTATE_ABOUT_AXIS
public static final int _ROTATE_BETWEEN_TWO_AXES
public static MoveFaceBuilder.Types valueOf(int value)
public static MoveFaceBuilder.Types valueOf(String name)
public static MoveFaceBuilder.Types[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.