public interface MoveCurveBuilder extends FeatureBuilder
MoveCurve
builder
SynchronousCurveCollection.createMoveCurveBuilder(nxopen.features.MoveCurve)
Property | Value |
---|---|
CurveFinder.ChamferEnabled | 0 |
CurveFinder.CoincidentVertexEnabled | 0 |
CurveFinder.CoincidentVertexSketchGroupEnabled | 0 |
CurveFinder.CollinearEnabled | 0 |
CurveFinder.CollinearSketchGroupEnabled | 0 |
CurveFinder.ConcentricEnabled | 0 |
CurveFinder.ConcentricSketchGroupEnabled | 0 |
CurveFinder.EqualRadiusEnabled | 0 |
CurveFinder.EqualRadiusSketchGroupEnabled | 0 |
CurveFinder.OffsetEnabled | 0 |
CurveFinder.OffsetSketchGroupEnabled | 0 |
CurveFinder.ParallelEnabled | 0 |
CurveFinder.ParallelSketchGroupEnabled | 0 |
CurveFinder.SymmetricEnabled | 0 |
CurveFinder.TangentEnabled | 0 |
CurveFinder.TangentSketchGroupEnabled | 0 |
CurveFinder.UseCurveFinder | 1 |
CurveFinder.VertexOnCurveEnabled | 0 |
CurveFinder.VertexOnCurveSketchGroupEnabled | 0 |
TransformMotion.DeltaEnum | ReferenceWcsWorkPart |
TransformMotion.DeltaXc.Value | 0.0 |
TransformMotion.DeltaYc.Value | 0.0 |
TransformMotion.DeltaZc.Value | 0.0 |
TransformMotion.Option | Dynamic |
Modifier and Type | Method and Description |
---|---|
CurveFinderBuilder |
curveFinder()
Returns the curve section
License requirements: None. |
double |
distanceTolerance()
Returns the distance tolerance
License requirements: None. |
boolean |
keepOrthogonal()
Returns a value that indicates whether keep orthogonal is enabled
License requirements: None. |
int |
keepTangent()
Returns a value that indicates which keep tangent support is selected
License requirements: None. |
void |
setDistanceTolerance(double distanceTolerance)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
void |
setKeepOrthogonal(boolean keepOrthogonal)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
void |
setKeepTangent(int keepTangent)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
void |
setSizeOption(int sizeOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
int |
sizeOption()
Returns a value that indicates which size option is selected
License requirements: None. |
ModlMotion |
transformMotion()
Returns the transform motion
License requirements: None. |
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
CurveFinderBuilder curveFinder() throws NXException, RemoteException
NXException
RemoteException
ModlMotion transformMotion() throws NXException, RemoteException
NXException
RemoteException
double distanceTolerance() throws NXException, RemoteException
NXException
RemoteException
void setDistanceTolerance(double distanceTolerance) throws NXException, RemoteException
distanceTolerance
- NXException
RemoteException
int sizeOption() throws NXException, RemoteException
NXException
RemoteException
void setSizeOption(int sizeOption) throws NXException, RemoteException
sizeOption
- NXException
RemoteException
int keepTangent() throws NXException, RemoteException
NXException
RemoteException
void setKeepTangent(int keepTangent) throws NXException, RemoteException
keepTangent
- NXException
RemoteException
boolean keepOrthogonal() throws NXException, RemoteException
NXException
RemoteException
void setKeepOrthogonal(boolean keepOrthogonal) throws NXException, RemoteException
keepOrthogonal
- NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.