public static class LabelChamferBuilder.ChamferType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EDGE_ANGLE_OFFSET |
static int |
_EDGE_OFFSET |
static int |
_FACE_OFFSET |
static int |
_VERTEX |
static LabelChamferBuilder.ChamferType |
EDGE_ANGLE_OFFSET |
static LabelChamferBuilder.ChamferType |
EDGE_OFFSET |
static LabelChamferBuilder.ChamferType |
FACE_OFFSET |
static LabelChamferBuilder.ChamferType |
VERTEX |
Modifier and Type | Method and Description |
---|---|
static LabelChamferBuilder.ChamferType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LabelChamferBuilder.ChamferType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LabelChamferBuilder.ChamferType[] |
values()
Returns an array that contains the values for this enum.
|
public static final LabelChamferBuilder.ChamferType EDGE_OFFSET
public static final LabelChamferBuilder.ChamferType FACE_OFFSET
public static final LabelChamferBuilder.ChamferType EDGE_ANGLE_OFFSET
public static final LabelChamferBuilder.ChamferType VERTEX
public static final int _EDGE_OFFSET
public static final int _FACE_OFFSET
public static final int _EDGE_ANGLE_OFFSET
public static final int _VERTEX
public static LabelChamferBuilder.ChamferType valueOf(int value)
public static LabelChamferBuilder.ChamferType valueOf(String name)
public static LabelChamferBuilder.ChamferType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.