public static class IFormBuilder.ParameterDirectionOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ISO_U
Iso-U direction
|
static int |
_ISO_V
Iso-V direction
|
static IFormBuilder.ParameterDirectionOptions |
ISO_U
Iso-U direction
|
static IFormBuilder.ParameterDirectionOptions |
ISO_V
Iso-V direction
|
Modifier and Type | Method and Description |
---|---|
static IFormBuilder.ParameterDirectionOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static IFormBuilder.ParameterDirectionOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static IFormBuilder.ParameterDirectionOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final IFormBuilder.ParameterDirectionOptions ISO_U
public static final IFormBuilder.ParameterDirectionOptions ISO_V
public static final int _ISO_U
public static final int _ISO_V
public static IFormBuilder.ParameterDirectionOptions valueOf(int value)
public static IFormBuilder.ParameterDirectionOptions valueOf(String name)
public static IFormBuilder.ParameterDirectionOptions[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.