public static class GlobalShapingBuilder.TargetCurveOrientationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_PARALLEL
Target curve is parallel to the limit curves.
|
static int |
_PERPENDICULAR
Target curves are perpendicular to the limit curves.
|
static GlobalShapingBuilder.TargetCurveOrientationType |
PARALLEL
Target curve is parallel to the limit curves.
|
static GlobalShapingBuilder.TargetCurveOrientationType |
PERPENDICULAR
Target curves are perpendicular to the limit curves.
|
Modifier and Type | Method and Description |
---|---|
static GlobalShapingBuilder.TargetCurveOrientationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GlobalShapingBuilder.TargetCurveOrientationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GlobalShapingBuilder.TargetCurveOrientationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final GlobalShapingBuilder.TargetCurveOrientationType PARALLEL
public static final GlobalShapingBuilder.TargetCurveOrientationType PERPENDICULAR
public static final int _PARALLEL
public static final int _PERPENDICULAR
public static GlobalShapingBuilder.TargetCurveOrientationType valueOf(int value)
public static GlobalShapingBuilder.TargetCurveOrientationType valueOf(String name)
public static GlobalShapingBuilder.TargetCurveOrientationType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.