public interface FlowBlendBuilder extends FeatureBuilder
FlowBlend
builder
FeatureCollection.createFlowBlendBuilder(nxopen.features.FlowBlend)
Property | Value |
---|---|
Patch | 1 |
Trim (deprecated) | 0 |
Modifier and Type | Method and Description |
---|---|
VariableRadiusPointsBuilderList |
controlPoint()
Returns the control point object
License requirements: None. |
ScCollector |
edgeToBlend()
Returns the edge to blend
License requirements: None. |
VariableRadiusPointsBuilder |
newControlPoint()
The control point object's create function
License requirements: solid_modeling ("SOLIDS MODELING") . |
SmoothRangeBuilder |
newSmoothRange()
The smooth range object's create function
License requirements: solid_modeling ("SOLIDS MODELING") . |
boolean |
patch()
Returns the toggle to specify patch to body or not
License requirements: None. |
void |
setPatch(boolean patch)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
setTolerance(double tolerance)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
setTrim(boolean trim)
Deprecated.
Deprecated in NX10.0.1. This functionality is no longer supported.
|
SmoothRangeBuilderList |
smoothRange()
Returns the smooth range object
License requirements: None. |
double |
tolerance()
Returns the tolerance
License requirements: None. |
boolean |
trim()
Deprecated.
Deprecated in NX10.0.1. This functionality is no longer supported.
|
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
ScCollector edgeToBlend() throws NXException, RemoteException
NXException
RemoteException
VariableRadiusPointsBuilderList controlPoint() throws NXException, RemoteException
NXException
RemoteException
VariableRadiusPointsBuilder newControlPoint() throws NXException, RemoteException
NXException
RemoteException
SmoothRangeBuilderList smoothRange() throws NXException, RemoteException
NXException
RemoteException
SmoothRangeBuilder newSmoothRange() throws NXException, RemoteException
NXException
RemoteException
boolean trim() throws NXException, RemoteException
NXException
RemoteException
void setTrim(boolean trim) throws NXException, RemoteException
trim
- NXException
RemoteException
boolean patch() throws NXException, RemoteException
NXException
RemoteException
void setPatch(boolean patch) throws NXException, RemoteException
patch
- NXException
RemoteException
double tolerance() throws NXException, RemoteException
NXException
RemoteException
void setTolerance(double tolerance) throws NXException, RemoteException
tolerance
- NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.