public static class FlatteningAndFormingBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CALCULATION
This option faces to be flattened will be used to calculate the mapping.
|
static int |
_REUSE
This option uses a transformation maping of an existing flattening feature to reapply it in its original or reversed direction to additional transformation objects.
|
static FlatteningAndFormingBuilder.Types |
CALCULATION
This option faces to be flattened will be used to calculate the mapping.
|
static FlatteningAndFormingBuilder.Types |
REUSE
This option uses a transformation maping of an existing flattening feature to reapply it in its original or reversed direction to additional transformation objects.
|
Modifier and Type | Method and Description |
---|---|
static FlatteningAndFormingBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlatteningAndFormingBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlatteningAndFormingBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final FlatteningAndFormingBuilder.Types CALCULATION
public static final FlatteningAndFormingBuilder.Types REUSE
public static final int _CALCULATION
public static final int _REUSE
public static FlatteningAndFormingBuilder.Types valueOf(int value)
public static FlatteningAndFormingBuilder.Types valueOf(String name)
public static FlatteningAndFormingBuilder.Types[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.