public interface FixedBuilder extends FeatureBuilder
FeatureCollection.createFixedBuilder(nxopen.features.Fixed)
Property | Value |
---|---|
FaceToFix.CoaxialEnabled | 0 |
FaceToFix.CoplanarAxesEnabled | 0 |
FaceToFix.CoplanarEnabled | 0 |
FaceToFix.EqualDiameterEnabled | 0 |
FaceToFix.OffsetEnabled | 0 |
FaceToFix.ParallelEnabled | 0 |
FaceToFix.PerpendicularEnabled | 0 |
FaceToFix.SymmetricEnabled | 0 |
FaceToFix.TangentEnabled | 0 |
FaceToFix.ThicknessChainEnabled | 0 |
FaceToFix.UseFaceBrowse | 1 |
Modifier and Type | Method and Description |
---|---|
FaceRecognitionBuilder |
faceToFix()
Returns the face recognition builder holding the faces to be fixed.
|
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
FaceRecognitionBuilder faceToFix() throws NXException, RemoteException
FaceRecognitionBuilder
for details.
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.