public static class FaceBlendBuilder.DefiningType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BLEND_THREE_FACE
this is form new three face blend
|
static int |
_BLEND_TWO_FACE
this is for normal two face blend
|
static FaceBlendBuilder.DefiningType |
BLEND_THREE_FACE
this is form new three face blend
|
static FaceBlendBuilder.DefiningType |
BLEND_TWO_FACE
this is for normal two face blend
|
Modifier and Type | Method and Description |
---|---|
static FaceBlendBuilder.DefiningType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FaceBlendBuilder.DefiningType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FaceBlendBuilder.DefiningType[] |
values()
Returns an array that contains the values for this enum.
|
public static final FaceBlendBuilder.DefiningType BLEND_TWO_FACE
public static final FaceBlendBuilder.DefiningType BLEND_THREE_FACE
public static final int _BLEND_TWO_FACE
public static final int _BLEND_THREE_FACE
public static FaceBlendBuilder.DefiningType valueOf(int value)
public static FaceBlendBuilder.DefiningType valueOf(String name)
public static FaceBlendBuilder.DefiningType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.