public static class DatumPlaneBuilder.AlternateSolution extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BINORMAL
Datum plane at binormal to curve
|
static int |
_NORMAL
Datum plane at normal to curve
|
static int |
_OPPOSITE_BINORMAL
Datum plane at opposite to binormal to curve
|
static int |
_OPPOSITE_NORMAL
Datum plane at opposite to normal to curve
|
static int |
_OPPOSITE_TANGENT
Datum plane at opposite to tangent to curve
|
static int |
_PROJECT
This direction is calculated by projecting a point selected along a curve
to a line, a datum axis, an edge of a solid, a planar face or a datum plane
|
static int |
_PROJECT_VIEW
Datum plane direction is calculated during creation based on the view plane.
|
static int |
_TANGENT
Indicates the datum plane as tangent to curve
|
static DatumPlaneBuilder.AlternateSolution |
BINORMAL
Datum plane at binormal to curve
|
static DatumPlaneBuilder.AlternateSolution |
NORMAL
Datum plane at normal to curve
|
static DatumPlaneBuilder.AlternateSolution |
OPPOSITE_BINORMAL
Datum plane at opposite to binormal to curve
|
static DatumPlaneBuilder.AlternateSolution |
OPPOSITE_NORMAL
Datum plane at opposite to normal to curve
|
static DatumPlaneBuilder.AlternateSolution |
OPPOSITE_TANGENT
Datum plane at opposite to tangent to curve
|
static DatumPlaneBuilder.AlternateSolution |
PROJECT
This direction is calculated by projecting a point selected along a curve
to a line, a datum axis, an edge of a solid, a planar face or a datum plane
|
static DatumPlaneBuilder.AlternateSolution |
PROJECT_VIEW
Datum plane direction is calculated during creation based on the view plane.
|
static DatumPlaneBuilder.AlternateSolution |
TANGENT
Indicates the datum plane as tangent to curve
|
Modifier and Type | Method and Description |
---|---|
static DatumPlaneBuilder.AlternateSolution |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumPlaneBuilder.AlternateSolution |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumPlaneBuilder.AlternateSolution[] |
values()
Returns an array that contains the values for this enum.
|
public static final DatumPlaneBuilder.AlternateSolution TANGENT
public static final DatumPlaneBuilder.AlternateSolution NORMAL
public static final DatumPlaneBuilder.AlternateSolution BINORMAL
public static final DatumPlaneBuilder.AlternateSolution OPPOSITE_TANGENT
public static final DatumPlaneBuilder.AlternateSolution OPPOSITE_NORMAL
public static final DatumPlaneBuilder.AlternateSolution OPPOSITE_BINORMAL
public static final DatumPlaneBuilder.AlternateSolution PROJECT
public static final DatumPlaneBuilder.AlternateSolution PROJECT_VIEW
public static final int _TANGENT
public static final int _NORMAL
public static final int _BINORMAL
public static final int _OPPOSITE_TANGENT
public static final int _OPPOSITE_NORMAL
public static final int _OPPOSITE_BINORMAL
public static final int _PROJECT
public static final int _PROJECT_VIEW
public static DatumPlaneBuilder.AlternateSolution valueOf(int value)
public static DatumPlaneBuilder.AlternateSolution valueOf(String name)
public static DatumPlaneBuilder.AlternateSolution[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.