public static class BridgeCurveBuilder.CurveFitTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ADVANCED
general fit curve
|
static int |
_CUBIC
fit curve with 3 degrees
|
static int |
_QUINTIC
fit curve with 5 degrees
|
static BridgeCurveBuilder.CurveFitTypes |
ADVANCED
general fit curve
|
static BridgeCurveBuilder.CurveFitTypes |
CUBIC
fit curve with 3 degrees
|
static BridgeCurveBuilder.CurveFitTypes |
QUINTIC
fit curve with 5 degrees
|
Modifier and Type | Method and Description |
---|---|
static BridgeCurveBuilder.CurveFitTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilder.CurveFitTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilder.CurveFitTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final BridgeCurveBuilder.CurveFitTypes CUBIC
public static final BridgeCurveBuilder.CurveFitTypes QUINTIC
public static final BridgeCurveBuilder.CurveFitTypes ADVANCED
public static final int _CUBIC
public static final int _QUINTIC
public static final int _ADVANCED
public static BridgeCurveBuilder.CurveFitTypes valueOf(int value)
public static BridgeCurveBuilder.CurveFitTypes valueOf(String name)
public static BridgeCurveBuilder.CurveFitTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.