public interface AngularDimBuilder extends DimensionBuilder
AngularDim
builder
FeatureCollection.createAngularDimensionBuilder(nxopen.features.AngularDim)
Modifier and Type | Method and Description |
---|---|
boolean |
alternativeAngle()
Returns the alternative angle toggle allows you to compute angle that is 360 degree subtracts current angle
License requirements: None. |
boolean |
complementAngleFlag()
Returns the complement angle flag
License requirements: None. |
boolean |
getIsComplementAngle(Point3d dimensionLocation)
Returns the flag indicating if angle is complement
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
SelectNXObject |
measurementObject()
Returns the measurement object is for the move object
License requirements: None. |
SelectNXObject |
originObject()
Returns the origin object is for the fixed object
License requirements: None. |
void |
setAlternativeAngle(boolean alternativeAngle)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
setComplementAngleFlag(boolean complementAngleFlag)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
setInterpartSourceEdge(Edge interpartSourceEdge)
Sets the interpart source edge
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
dimensionLocation, faceChangeOverflowBehavior, facesToMove, getDimension, saveConstraints, value
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
SelectNXObject originObject() throws NXException, RemoteException
NXException
RemoteException
SelectNXObject measurementObject() throws NXException, RemoteException
NXException
RemoteException
boolean alternativeAngle() throws NXException, RemoteException
NXException
RemoteException
void setAlternativeAngle(boolean alternativeAngle) throws NXException, RemoteException
alternativeAngle
- NXException
RemoteException
boolean complementAngleFlag() throws NXException, RemoteException
NXException
RemoteException
void setComplementAngleFlag(boolean complementAngleFlag) throws NXException, RemoteException
complementAngleFlag
- NXException
RemoteException
boolean getIsComplementAngle(Point3d dimensionLocation) throws NXException, RemoteException
dimensionLocation
- Indicates dimension origin cursor locationNXException
RemoteException
void setInterpartSourceEdge(Edge interpartSourceEdge) throws NXException, RemoteException
interpartSourceEdge
- edgeNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.