public static class AestheticFaceBlendBuilder.ShapeType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ACCELERATED
Accelerated option will generate more shapes depending on the size of the center radius and continuity specified.
|
static int |
_CIRCULAR
Circular option will always generate a constant radius arc shape.
|
static AestheticFaceBlendBuilder.ShapeType |
ACCELERATED
Accelerated option will generate more shapes depending on the size of the center radius and continuity specified.
|
static AestheticFaceBlendBuilder.ShapeType |
CIRCULAR
Circular option will always generate a constant radius arc shape.
|
Modifier and Type | Method and Description |
---|---|
static AestheticFaceBlendBuilder.ShapeType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AestheticFaceBlendBuilder.ShapeType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AestheticFaceBlendBuilder.ShapeType[] |
values()
Returns an array that contains the values for this enum.
|
public static final AestheticFaceBlendBuilder.ShapeType ACCELERATED
public static final AestheticFaceBlendBuilder.ShapeType CIRCULAR
public static final int _ACCELERATED
public static final int _CIRCULAR
public static AestheticFaceBlendBuilder.ShapeType valueOf(int value)
public static AestheticFaceBlendBuilder.ShapeType valueOf(String name)
public static AestheticFaceBlendBuilder.ShapeType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.