public interface AdmMoveFaceBuilder extends FeatureBuilder
AdmMoveFace
builder
FeatureCollection.createAdmMoveFaceBuilder(nxopen.features.AdmMoveFace)
Property | Value |
---|---|
FaceToMove.CoaxialEnabled | 0 |
FaceToMove.CoplanarAxesEnabled | 0 |
FaceToMove.CoplanarEnabled | 0 |
FaceToMove.EqualDiameterEnabled | 0 |
FaceToMove.OffsetEnabled | 0 |
FaceToMove.ParallelEnabled | 0 |
FaceToMove.PerpendicularEnabled | 0 |
FaceToMove.SymmetricEnabled | 0 |
FaceToMove.TangentEnabled | 0 |
FaceToMove.ThicknessChainEnabled | 0 |
FaceToMove.UseFaceBrowse | 1 |
HealOption | True |
Motion.DeltaEnum | ReferenceWcsWorkPart |
Motion.DeltaXc.Value | 0.0 |
Motion.DeltaYc.Value | 0.0 |
Motion.DeltaZc.Value | 0.0 |
Motion.Option | DistanceAngle |
StepOption.StepOption | None |
Modifier and Type | Interface and Description |
---|---|
static class |
AdmMoveFaceBuilder.MoveOptionType
Represents the move option.
|
Modifier and Type | Method and Description |
---|---|
FaceChangeOverflowBehavior |
faceChangeOverflowBehavior()
Returns the face change overflow behavior.
|
FaceRecognitionBuilder |
faceToMove()
Returns the face to move.
|
boolean |
healOption()
Returns the heal option.
|
ModlMotion |
motion()
Returns the motion.
|
AdmMoveFaceBuilder.MoveOptionType |
moveOption()
Returns the move option.
|
boolean |
pasteOption()
Returns the paste option.
|
void |
setHealOption(boolean healOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
setMoveOption(AdmMoveFaceBuilder.MoveOptionType moveOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
setPasteOption(boolean pasteOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
StepOptionBehavior |
stepOption()
Returns the step option behavior.
|
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
FaceRecognitionBuilder faceToMove() throws NXException, RemoteException
FaceRecognitionBuilder
for details.
NXException
RemoteException
ModlMotion motion() throws NXException, RemoteException
ModlMotion
for details.
NXException
RemoteException
FaceChangeOverflowBehavior faceChangeOverflowBehavior() throws NXException, RemoteException
FaceChangeOverflowBehavior
for details.
NXException
RemoteException
StepOptionBehavior stepOption() throws NXException, RemoteException
StepOptionBehavior
for details.
NXException
RemoteException
AdmMoveFaceBuilder.MoveOptionType moveOption() throws NXException, RemoteException
NXException
RemoteException
void setMoveOption(AdmMoveFaceBuilder.MoveOptionType moveOption) throws NXException, RemoteException
moveOption
- NXException
RemoteException
boolean pasteOption() throws NXException, RemoteException
NXException
RemoteException
void setPasteOption(boolean pasteOption) throws NXException, RemoteException
pasteOption
- NXException
RemoteException
boolean healOption() throws NXException, RemoteException
NXException
RemoteException
void setHealOption(boolean healOption) throws NXException, RemoteException
healOption
- NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.