public interface DynamicSectionCut extends NXObject
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
INXObject |
cutObject()
Returns the object from which this section-cut is generated.
|
void |
prepareForMeasure(NXObject contextOccurrence,
View view)
Prepares the section-cut for measurement.
|
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
INXObject cutObject() throws NXException, RemoteException
NXException
RemoteException
void prepareForMeasure(NXObject contextOccurrence, View view) throws NXException, RemoteException
Session.deleteTransientDynamicSectionCutData()
.
contextOccurrence
- This can be null. If non null, then this must
be an occurrence in the part of section-cut occurrence.
In this case, occurrences of curves associated with the
section-cut are setup for measurement.view
- This can be null. If a valid view is specified,
then it is used to skip invisible body occurrences in a
component for creation of curves used for measurement.
If curves have already been created, then view is ignored.NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.