public interface DrawDiePunchBuilder extends FeatureBuilder
DieCollection.drawDiePunch(nxopen.features.Feature)
Modifier and Type | Interface and Description |
---|---|
static class |
DrawDiePunchBuilder.PunchProfileData
This class holds the data returned from
getPunchProfile() |
Modifier and Type | Method and Description |
---|---|
boolean |
alignStartOrientation()
Returns the align start orientation switch of the draw die punch casting, if true use the alignment point to define the start of the punch profile,
if false use the default algorithm to define the start of the punch profile.
|
double |
angleTolerance()
Returns the angle tolerance of the draw die punch casting.
|
ISurface |
baseOrientation()
Returns the base orientation of the draw die punch casting.
|
HoleParentBuilder |
boltHoleParent()
Returns the bolt hole parent builder of the draw die punch.
|
CastReliefParentBuilder |
castReliefParent()
Returns the cast relief builder of the draw die punch.
|
IOrientation |
closedStartOrientation()
Returns the closed start orientation of the draw die punch casting.
|
HoleParentBuilder |
coordinatingHoleParent()
Returns the coordinating hole parent builder of the draw die punch.
|
boolean |
corePunch()
Returns the core punch switch of the draw die punch casting, if true the punch will be cored, if false the punch will not be cored.
|
DeckParentBuilder |
deckParent()
Returns the deck builder of the draw die punch.
|
CartesianCoordinateSystem |
dieCenterlineCsys()
Returns the die centerline csys of the draw die punch casting.
|
boolean |
displayHoles()
Returns the display holes switch of the draw die punch casting, if true holes will be created in the punch, if false holes will not be created.
|
double |
distanceTolerance()
Returns the distance tolerance of the draw die punch casting.
|
HoleParentBuilder |
dowelHoleParent()
Returns the dowel hole parent builder of the draw die punch.
|
DrawDiePunchBuilder.PunchProfileData |
getPunchProfile()
Gets the punch profile of the draw die punch casting.
|
HandlingCoreParentBuilder |
handlingCoreParent()
Returns the handling core parent builder of the draw die punch.
|
KeywayParentBuilder |
keywayParent()
Returns the keyway parent builder of the draw die punch.
|
RibParentBuilder |
partialRibbingParent()
Returns the partial ribbing parent builder of the draw die punch.
|
boolean |
preliminaryBuild()
Returns the preliminary build switch of the draw die punch casting, if true the fast build options will be used,
if false accurate build options will be used.
|
PressureSystemParentBuilder |
pressureSystemParent()
Returns the pressure system parent builder of the draw die punch.
|
PointParentBuilder |
pressureSystemReversalParent()
Returns the pressure system reversal parent builder of the draw die punch.
|
RibParentBuilder |
ribbingParent()
Returns the ribbing parent builder of the draw die punch.
|
DrawDiePunchSectionBuilder |
section()
Returns the section builder of the draw die punch.
|
void |
setAlignStartOrientation(boolean alignStartOrientation)
Sets the align start orientation switch of the draw die punch casting, if true use the alignment point to define the start of the punch profile,
if false use the default algorithm to define the start of the punch profile.
|
void |
setAngleTolerance(double angleTolerance)
Sets the angle tolerance of the draw die punch casting.
|
void |
setBaseOrientation(ISurface baseOrientation)
Sets the base orientation of the draw die punch casting.
|
void |
setClosedStartOrientation(IOrientation closedStartOrientation)
Sets the closed start orientation of the draw die punch casting.
|
void |
setCorePunch(boolean corePunch)
Sets the core punch switch of the draw die punch casting, if true the punch will be cored, if false the punch will not be cored.
|
void |
setDieCenterlineCsys(CartesianCoordinateSystem dieCenterlineCsys)
Sets the die centerline csys of the draw die punch casting.
|
void |
setDisplayHoles(boolean displayHoles)
Sets the display holes switch of the draw die punch casting, if true holes will be created in the punch, if false holes will not be created.
|
void |
setDistanceTolerance(double distanceTolerance)
Sets the distance tolerance of the draw die punch casting.
|
void |
setPreliminaryBuild(boolean preliminaryBuild)
Sets the preliminary build switch of the draw die punch casting, if true the fast build options will be used,
if false accurate build options will be used.
|
void |
setPunchProfile(DirectionOption direction,
IProfile[] profileEntries)
Sets the punch profile of the draw die punch casting.
|
void |
setSheetMetal(Body sheetMetal)
Sets the sheet metal of the draw die punch casting.
|
Body |
sheetMetal()
Returns the sheet metal of the draw die punch casting.
|
RibParentBuilder |
strengtheningRibbingParent()
Returns the strengthening ribbing parent builder of the draw die punch.
|
HoleParentBuilder |
ventHoleParent()
Returns the vent hole parent builder of the draw die punch.
|
PadParentBuilder |
wearPlateParent()
Returns the wear plate parent builder of the draw die punch.
|
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
void setPunchProfile(DirectionOption direction, IProfile[] profileEntries) throws NXException, RemoteException
direction
- Profile direction.profileEntries
- The profile entries, can be curves, edges, faces, sketches or curve features.NXException
RemoteException
DrawDiePunchBuilder.PunchProfileData getPunchProfile() throws NXException, RemoteException
NXException
RemoteException
void setBaseOrientation(ISurface baseOrientation) throws NXException, RemoteException
baseOrientation
- NXException
RemoteException
ISurface baseOrientation() throws NXException, RemoteException
NXException
RemoteException
void setSheetMetal(Body sheetMetal) throws NXException, RemoteException
sheetMetal
- NXException
RemoteException
Body sheetMetal() throws NXException, RemoteException
NXException
RemoteException
void setDieCenterlineCsys(CartesianCoordinateSystem dieCenterlineCsys) throws NXException, RemoteException
dieCenterlineCsys
- NXException
RemoteException
CartesianCoordinateSystem dieCenterlineCsys() throws NXException, RemoteException
NXException
RemoteException
void setClosedStartOrientation(IOrientation closedStartOrientation) throws NXException, RemoteException
closedStartOrientation
- NXException
RemoteException
IOrientation closedStartOrientation() throws NXException, RemoteException
NXException
RemoteException
void setCorePunch(boolean corePunch) throws NXException, RemoteException
corePunch
- NXException
RemoteException
boolean corePunch() throws NXException, RemoteException
NXException
RemoteException
void setDisplayHoles(boolean displayHoles) throws NXException, RemoteException
displayHoles
- NXException
RemoteException
boolean displayHoles() throws NXException, RemoteException
NXException
RemoteException
void setPreliminaryBuild(boolean preliminaryBuild) throws NXException, RemoteException
preliminaryBuild
- NXException
RemoteException
boolean preliminaryBuild() throws NXException, RemoteException
NXException
RemoteException
void setAlignStartOrientation(boolean alignStartOrientation) throws NXException, RemoteException
alignStartOrientation
- NXException
RemoteException
boolean alignStartOrientation() throws NXException, RemoteException
NXException
RemoteException
void setDistanceTolerance(double distanceTolerance) throws NXException, RemoteException
distanceTolerance
- NXException
RemoteException
double distanceTolerance() throws NXException, RemoteException
NXException
RemoteException
void setAngleTolerance(double angleTolerance) throws NXException, RemoteException
angleTolerance
- NXException
RemoteException
double angleTolerance() throws NXException, RemoteException
NXException
RemoteException
DrawDiePunchSectionBuilder section() throws NXException, RemoteException
NXException
RemoteException
HoleParentBuilder ventHoleParent() throws NXException, RemoteException
NXException
RemoteException
HoleParentBuilder coordinatingHoleParent() throws NXException, RemoteException
NXException
RemoteException
RibParentBuilder ribbingParent() throws NXException, RemoteException
NXException
RemoteException
RibParentBuilder partialRibbingParent() throws NXException, RemoteException
NXException
RemoteException
HandlingCoreParentBuilder handlingCoreParent() throws NXException, RemoteException
NXException
RemoteException
KeywayParentBuilder keywayParent() throws NXException, RemoteException
NXException
RemoteException
HoleParentBuilder dowelHoleParent() throws NXException, RemoteException
NXException
RemoteException
HoleParentBuilder boltHoleParent() throws NXException, RemoteException
NXException
RemoteException
PressureSystemParentBuilder pressureSystemParent() throws NXException, RemoteException
NXException
RemoteException
PointParentBuilder pressureSystemReversalParent() throws NXException, RemoteException
NXException
RemoteException
PadParentBuilder wearPlateParent() throws NXException, RemoteException
NXException
RemoteException
CastReliefParentBuilder castReliefParent() throws NXException, RemoteException
NXException
RemoteException
DeckParentBuilder deckParent() throws NXException, RemoteException
NXException
RemoteException
RibParentBuilder strengtheningRibbingParent() throws NXException, RemoteException
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.