public class DirectionOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FROM_END
Profile direction is aligned with the first curve from the end to start.
|
static int |
_FROM_START
Profile direction is aligned with the first curve from the start to end.
|
static DirectionOption |
FROM_END
Profile direction is aligned with the first curve from the end to start.
|
static DirectionOption |
FROM_START
Profile direction is aligned with the first curve from the start to end.
|
Modifier and Type | Method and Description |
---|---|
static DirectionOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DirectionOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DirectionOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final DirectionOption FROM_END
public static final DirectionOption FROM_START
public static final int _FROM_END
public static final int _FROM_START
public static DirectionOption valueOf(int value)
public static DirectionOption valueOf(String name)
public static DirectionOption[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.