Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
Arc[] |
Sketch.FilletData.fillets
The fillet arcs that are created.
|
Modifier and Type | Method and Description |
---|---|
Arc |
CurveCollection.createArc(Point3d center,
NXMatrix matrix,
double radius,
double startAngle,
double endAngle)
Creates an
Arc . |
Arc |
CurveCollection.createArc(Point3d startPoint,
Point3d pointOn,
Point3d endPoint,
boolean alternateSolution)
Creates an
Arc that passes through the three specified points. |
Arc |
CurveCollection.createArc(Point3d center,
Vector3d xDirection,
Vector3d yDirection,
double radius,
double startAngle,
double endAngle)
Creates an
Arc . |
Arc |
ArcCollection.findObject(String journalIdentifier)
Finds the
Arc with the given identifier as recorded in a journal. |
Modifier and Type | Method and Description |
---|---|
void |
OrderedSelection.add(Arc entity,
boolean flipDirection)
Adds a arc to the list
License requirements: None. |
OrderedEdgeElemMethod |
SmartSelectionManager.createOrderedEdgeElemMethod(Arc seed,
boolean doEntityVisibilityCheck,
boolean flipSeedStart)
Creates a ordered edge elem method
License requirements: nx_masterfem ("Finite Element Modeling") . |
OrderedEdgeNodeMethod |
SmartSelectionManager.createOrderedEdgeNodeMethod(Arc seed,
boolean doEntityVisibilityCheck,
boolean flipSeedStart)
Creates a ordered edge node method
License requirements: nx_masterfem ("Finite Element Modeling") . |
RelatedElemMethod |
SmartSelectionManager.createRelatedElemMethod(Arc[] seedTags)
Deprecated.
Deprecated in NX11.0.0. Use overloaded
SmartSelectionManager.createRelatedElemMethod(nxopen.cae.Mesh) which takes as input an array of Arc objects and the argument doEntityVisibilityCheck.
|
RelatedElemMethod |
SmartSelectionManager.createRelatedElemMethod(Arc[] seedTags,
boolean doEntityVisibilityCheck)
Creates a related elem method
License requirements: nx_masterfem ("Finite Element Modeling") . |
RelatedNodeMethod |
SmartSelectionManager.createRelatedNodeMethod(Arc[] seedTags)
Deprecated.
Deprecated in NX11.0.0. Use overloaded
SmartSelectionManager.createRelatedNodeMethod(nxopen.cae.Mesh) which takes as input an array of Arc objects and the argument doEntityVisibilityCheck.
|
RelatedNodeMethod |
SmartSelectionManager.createRelatedNodeMethod(Arc[] seedTags,
boolean doEntityVisibilityCheck)
Creates a related node method
License requirements: nx_masterfem ("Finite Element Modeling") . |
Modifier and Type | Method and Description |
---|---|
AssociativeArcBuilder |
BaseFeatureCollection.createAssociativeArcBuilder(Arc nonAssociativeArc)
Creates a
AssociativeArcBuilder
License requirements: None. |
Modifier and Type | Interface and Description |
---|---|
interface |
ArcSegment
Represents a arc segment.
|
interface |
GapArcSegment
Represents a gap arc segment.
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.