public static class InspectionConstructedFeatureBuilder.DirectionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FEATURE
Use a feature (nominal/actual) for the vector
|
static int |
_RADIAL
Use a radial direction vector
|
static int |
_SPECIFIED_VECTOR
Use a user specified direction vector
|
static InspectionConstructedFeatureBuilder.DirectionType |
FEATURE
Use a feature (nominal/actual) for the vector
|
static InspectionConstructedFeatureBuilder.DirectionType |
RADIAL
Use a radial direction vector
|
static InspectionConstructedFeatureBuilder.DirectionType |
SPECIFIED_VECTOR
Use a user specified direction vector
|
Modifier and Type | Method and Description |
---|---|
static InspectionConstructedFeatureBuilder.DirectionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionConstructedFeatureBuilder.DirectionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionConstructedFeatureBuilder.DirectionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionConstructedFeatureBuilder.DirectionType SPECIFIED_VECTOR
public static final InspectionConstructedFeatureBuilder.DirectionType RADIAL
public static final InspectionConstructedFeatureBuilder.DirectionType FEATURE
public static final int _SPECIFIED_VECTOR
public static final int _RADIAL
public static final int _FEATURE
public static InspectionConstructedFeatureBuilder.DirectionType valueOf(int value)
public static InspectionConstructedFeatureBuilder.DirectionType valueOf(String name)
public static InspectionConstructedFeatureBuilder.DirectionType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.