public static class InspectionConstructedFeatureBuilder.DestPcsEnumType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ACTUAL_PCS
Use a user specified actual PCS as the destination
|
static int |
_CURRENT_PCS
Use current PCS as the destination
|
static int |
_NOMINAL_PCS
Use a user specified nominal PCS as the destination
|
static InspectionConstructedFeatureBuilder.DestPcsEnumType |
ACTUAL_PCS
Use a user specified actual PCS as the destination
|
static InspectionConstructedFeatureBuilder.DestPcsEnumType |
CURRENT_PCS
Use current PCS as the destination
|
static InspectionConstructedFeatureBuilder.DestPcsEnumType |
NOMINAL_PCS
Use a user specified nominal PCS as the destination
|
Modifier and Type | Method and Description |
---|---|
static InspectionConstructedFeatureBuilder.DestPcsEnumType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionConstructedFeatureBuilder.DestPcsEnumType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionConstructedFeatureBuilder.DestPcsEnumType[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionConstructedFeatureBuilder.DestPcsEnumType CURRENT_PCS
public static final InspectionConstructedFeatureBuilder.DestPcsEnumType NOMINAL_PCS
public static final InspectionConstructedFeatureBuilder.DestPcsEnumType ACTUAL_PCS
public static final int _CURRENT_PCS
public static final int _NOMINAL_PCS
public static final int _ACTUAL_PCS
public static InspectionConstructedFeatureBuilder.DestPcsEnumType valueOf(int value)
public static InspectionConstructedFeatureBuilder.DestPcsEnumType valueOf(String name)
public static InspectionConstructedFeatureBuilder.DestPcsEnumType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.