public static class ResultProbeBuilder.SelectionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BODIES |
static int |
_EDGES |
static int |
_ELEMENTS |
static int |
_ENTIRE_MODEL |
static int |
_FACES |
static int |
_NODES |
static int |
_NONE |
static int |
_POINTS |
static int |
_QUERY_CURVE |
static ResultProbeBuilder.SelectionType |
BODIES |
static ResultProbeBuilder.SelectionType |
EDGES |
static ResultProbeBuilder.SelectionType |
ELEMENTS |
static ResultProbeBuilder.SelectionType |
ENTIRE_MODEL |
static ResultProbeBuilder.SelectionType |
FACES |
static ResultProbeBuilder.SelectionType |
NODES |
static ResultProbeBuilder.SelectionType |
NONE |
static ResultProbeBuilder.SelectionType |
POINTS |
static ResultProbeBuilder.SelectionType |
QUERY_CURVE |
Modifier and Type | Method and Description |
---|---|
static ResultProbeBuilder.SelectionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ResultProbeBuilder.SelectionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ResultProbeBuilder.SelectionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ResultProbeBuilder.SelectionType ENTIRE_MODEL
public static final ResultProbeBuilder.SelectionType NODES
public static final ResultProbeBuilder.SelectionType ELEMENTS
public static final ResultProbeBuilder.SelectionType POINTS
public static final ResultProbeBuilder.SelectionType EDGES
public static final ResultProbeBuilder.SelectionType FACES
public static final ResultProbeBuilder.SelectionType BODIES
public static final ResultProbeBuilder.SelectionType QUERY_CURVE
public static final ResultProbeBuilder.SelectionType NONE
public static final int _ENTIRE_MODEL
public static final int _NODES
public static final int _ELEMENTS
public static final int _POINTS
public static final int _EDGES
public static final int _FACES
public static final int _BODIES
public static final int _QUERY_CURVE
public static final int _NONE
public static ResultProbeBuilder.SelectionType valueOf(int value)
public static ResultProbeBuilder.SelectionType valueOf(String name)
public static ResultProbeBuilder.SelectionType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.