public static class ResultProbeBuilder.NodalCombination extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ARITHMETIC_MEAN |
static int |
_MAXIMUM |
static int |
_MINIMUM |
static int |
_SUM |
static ResultProbeBuilder.NodalCombination |
ARITHMETIC_MEAN |
static ResultProbeBuilder.NodalCombination |
MAXIMUM |
static ResultProbeBuilder.NodalCombination |
MINIMUM |
static ResultProbeBuilder.NodalCombination |
SUM |
Modifier and Type | Method and Description |
---|---|
static ResultProbeBuilder.NodalCombination |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ResultProbeBuilder.NodalCombination |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ResultProbeBuilder.NodalCombination[] |
values()
Returns an array that contains the values for this enum.
|
public static final ResultProbeBuilder.NodalCombination ARITHMETIC_MEAN
public static final ResultProbeBuilder.NodalCombination MINIMUM
public static final ResultProbeBuilder.NodalCombination MAXIMUM
public static final ResultProbeBuilder.NodalCombination SUM
public static final int _ARITHMETIC_MEAN
public static final int _MINIMUM
public static final int _MAXIMUM
public static final int _SUM
public static ResultProbeBuilder.NodalCombination valueOf(int value)
public static ResultProbeBuilder.NodalCombination valueOf(String name)
public static ResultProbeBuilder.NodalCombination[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.