Modifier and Type | Interface and Description |
---|---|
static class |
ModelCheckManager.CheckModelConsistencyData
This class holds the data returned from
checkModelConsistency(java.lang.String) |
Modifier and Type | Method and Description |
---|---|
ModelCheckManager.CheckModelConsistencyData |
checkModelConsistency(String logFileName)
|
AlignShellElementNormalBuilder |
createAlignShellElementNormalBuilder()
Provides access for creating align 2D element normal builders in a cae part
License requirements: nx_masterfem ("Finite Element Modeling") . |
DuplicateElementsCheckBuilder |
createDuplicateElementsCheckBuilder()
Provides access for creating duplicate elements builder in a cae part.
|
DuplicateNodesCheckBuilder |
createDuplicateNodesCheckBuilder()
Provides access for creating duplicate nodes builder in a cae part.
|
ElementEdgeCheckBuilder |
createElementEdgeCheckBuilder()
Provides access for creating Model Check builders in a cae part
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
ElementMaterialOrientationCheckBuilder |
createElementMaterialOrientationCheckBuilder()
Provides access for creating element material orientation builder in a cae part.
|
ElementQualityCheckBuilder |
createElementQualityCheckBuilder()
Provides access for creating element quality Check builders in a cae part
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
FaceClearanceCheckBuilder |
createFaceClearanceCheckBuilder()
Provides access for creating face clearance check builder in a
FemPart part. |
MechanicalLoadSumBuilder |
createMechanicalLoadSumBuilder()
Creates a builder for mechanical load summary command
License requirements: nx_masterfem ("Finite Element Modeling") . |
ModelSetupCheckBuilder |
createModelSetupCheckBuilder()
Provides access for creating model setup check builder in a
SimPart part
or AssyFemPart
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX8.5.0 |
ReverseShellElementNormalBuilder |
createReverseShellElementNormalBuilder()
Provides access for creating reverse 2D element normal builders in a cae part
License requirements: nx_masterfem ("Finite Element Modeling") . |
SolidElementFaceNormalBuilder |
createSolidElementFaceNormalBuilder()
Provides access for creating solid element face normal builder in a cae part
License requirements: nx_masterfem ("Finite Element Modeling") . |
SolidPropertyCheckBuilder |
createSolidPropertyCheckBuilder()
Creates a builder for solid properties check command
License requirements: nx_masterfem ("Finite Element Modeling") . |
MechanicalLoadSumBuilder createMechanicalLoadSumBuilder() throws NXException, RemoteException
NXException
RemoteException
SolidPropertyCheckBuilder createSolidPropertyCheckBuilder() throws NXException, RemoteException
NXException
RemoteException
ElementEdgeCheckBuilder createElementEdgeCheckBuilder() throws NXException, RemoteException
NXException
RemoteException
ReverseShellElementNormalBuilder createReverseShellElementNormalBuilder() throws NXException, RemoteException
NXException
RemoteException
AlignShellElementNormalBuilder createAlignShellElementNormalBuilder() throws NXException, RemoteException
NXException
RemoteException
SolidElementFaceNormalBuilder createSolidElementFaceNormalBuilder() throws NXException, RemoteException
NXException
RemoteException
DuplicateNodesCheckBuilder createDuplicateNodesCheckBuilder() throws NXException, RemoteException
BaseFemPart
part.
NXException
RemoteException
DuplicateElementsCheckBuilder createDuplicateElementsCheckBuilder() throws NXException, RemoteException
BaseFemPart
part.
NXException
RemoteException
FaceClearanceCheckBuilder createFaceClearanceCheckBuilder() throws NXException, RemoteException
FemPart
part.
NXException
RemoteException
ElementMaterialOrientationCheckBuilder createElementMaterialOrientationCheckBuilder() throws NXException, RemoteException
NXException
RemoteException
ElementQualityCheckBuilder createElementQualityCheckBuilder() throws NXException, RemoteException
NXException
RemoteException
ModelSetupCheckBuilder createModelSetupCheckBuilder() throws NXException, RemoteException
SimPart
part
or AssyFemPart
NXException
RemoteException
ModelCheckManager.CheckModelConsistencyData checkModelConsistency(String logFileName) throws NXException, RemoteException
CAEBody
in a FemPart
, to find
out the CAE bodies which is inconsistent to the master bodies, output the body list to log file or listing window
if there is no log file name specified.
If the master part is not loaded, a CaeGroup
is created to contain these failed bodies.
If the master part is loaded, continue to fix the inconsistent CAE bodies by deleting and recreating them.
The mesh recipes associated with the bodies will be deleted while fixing model consistency. A CaeGroup
is created to contain the bodies created newly
logFileName
- the full log file nameNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.