public interface AssyFemPart extends BaseFemPart
PartCollection
class to load or create a part. BaseFemPart.AxisymAbstractionType, BaseFemPart.SolverAndAnalysisTypeData
BasePart.BookmarkOption, BasePart.CloseAfterSave, BasePart.CloseModified, BasePart.CloseWholeTree, BasePart.CollaborativeContentType, BasePart.HistoryEventInformation, BasePart.IncompleteStatus, BasePart.PartPreview, BasePart.PreviewImageData, BasePart.ReopenData, BasePart.SaveComponents, BasePart.TransientStatus, BasePart.Units
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
void |
finalizeCreation(Part cadPart,
String solverTypeName,
String analysisTypeType,
BaseFemPart.AxisymAbstractionType abstractionType,
String[] description)
Deprecated.
Deprecated in NX11.0.0. Use
finalizeCreation(nxopen.Part, java.lang.String, java.lang.String, nxopen.cae.BaseFemPart.AxisymAbstractionType, java.lang.String[], boolean, nxopen.CoordinateSystem) that includes CyclicSymmetryCSYS instead.
|
void |
finalizeCreation(Part cadPart,
String solverTypeName,
String analysisTypeType,
BaseFemPart.AxisymAbstractionType abstractionType,
String[] description,
boolean useCyclicSymmetryCSYS,
CoordinateSystem cyclicSymmetryCsys)
Finalizes the creation of the assembly fem part file.
|
void |
finalizeCreation(Part cadPart,
String solverTypeName,
String analysisTypeType,
String[] description)
Deprecated.
Deprecated in NX9.0.0. Use
finalizeCreation(nxopen.Part, java.lang.String, java.lang.String, nxopen.cae.BaseFemPart.AxisymAbstractionType, java.lang.String[], boolean, nxopen.CoordinateSystem) that includes abstraction type instead.
|
Part |
masterCadPart()
Returns the master cad part associated with the assembly fem part
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
baseFEModel, fullPathForAssociatedCadPart, getAbstractionType, getCyclicSymmetryCsys, getEnableMeshMorph, getSolverAndAnalysisType, setCyclicSymmetryCsys, setEnableMeshMorph, setSolverAndAnalysisType, setSolverAndAnalysisTypeAndAbstraction, setUseCyclicSymmetryCsys, sketchCurves, useCyclicSymmetryCsys
boundingVolumes, caeGroups, caeQueryCurves, createModelDisplayBuilder, createSolverAppendOption, deleteSolverAppendOption, elementQualitySettings, exportJt, exportSimulation, getCsysFlattenedLabel, getDescription, importExistingSimulation, layoutStates, meshControlDisplayMgr, modelCheckMgr, modelingObjectPropertyTables, newBeamSectionOffsetOptions, newBeamSectionOptions, newBeamSectionOrientationOptions, newMaterialOptions, nodeElementInfoMgr, physicalPropertyTables, postScenarioMgr, selectElementMgr, setDescription, showHideMgr, smartSelectionMgr
analysisManager, arcs, assemblies, assemblyManager, assignPermanentName, axes, baseFeatures, cameras, camfeatures, canBeDisplayPart, cgfxAttrs, cgfxMattex, close, colors, completeStructure, componentAssembly, convertToPMIBuilderManager, coordinateSystems, createDynamicSectionBuilder, createEffectivityConditionBuilder, createEffectivityConditionBuilder, createFacetSettingsBuilder, createGatewayGroupBuilder, createPerspectiveOptionsBuilder, createReferenceSet, curves, datums, decals, deleteReferenceSet, designStudy, directions, dynamicSections, ellipses, expressionGroups, expressions, fieldManager, fonts, fullPath, functions, getAllReferenceSets, getCollaborativeContentType, getHistoryInformation, getIncompleteStatus, getMakeUniqueName, getPreviewImage, getTransientStatus, grids, hasWriteAccess, hyperbolas, imageCaptureManager, images, imagesData, infiniteLines, isFullyLoaded, isReadOnly, layerCategories, layers, layouts, leaf, lights, lines, loadFeatureDataForSelection, loadFully, loadThisPartFully, materialManager, measureManager, modelingViews, nxmatrices, offsets, optimization, parabolas, partPreviewMode, partUnits, pdmpart, planes, plotManager, pointClouds, points, polylines, preferences, propertiesManager, regenerateDisplayFacets, regenerateDisplayFacets, reinstateTransience, removeTransience, reopen, reopenAs, requirementChecks, requirements, reverseBlankAll, ruleManager, save, saveAs, saveBookmark, saveDisplayFacets, saveOptions, scalars, scCollectors, sections, selPref, setMakeUniqueName, setPartPreviewMode, setSaveDisplayFacets, setUniqueIdentifier, shedobjs, splines, trueStudioObjs, uniqueIdentifier, unitCollection, userDefinedObjectManager, validations, views, wcs, xforms
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
void finalizeCreation(Part cadPart, String solverTypeName, String analysisTypeType, BaseFemPart.AxisymAbstractionType abstractionType, String[] description, boolean useCyclicSymmetryCSYS, CoordinateSystem cyclicSymmetryCsys) throws NXException, RemoteException
cadPart
- the cad part to be associated with the fem partsolverTypeName
- the name of the solver. Refer to NX help for more informationanalysisTypeType
- the name of the analysis type. Refer to NX help for more informationabstractionType
- the axisymmetric abstraction type. Refer to NX help for more informationdescription
- descriptionuseCyclicSymmetryCSYS
- Use the selected cyclic symmetry csys or notcyclicSymmetryCsys
- tag of selected cyclic symmetry or nullNXException
RemoteException
void finalizeCreation(Part cadPart, String solverTypeName, String analysisTypeType, BaseFemPart.AxisymAbstractionType abstractionType, String[] description) throws NXException, RemoteException
finalizeCreation(nxopen.Part, java.lang.String, java.lang.String, nxopen.cae.BaseFemPart.AxisymAbstractionType, java.lang.String[], boolean, nxopen.CoordinateSystem)
that includes CyclicSymmetryCSYS instead.
cadPart
- the cad part to be associated with the fem partsolverTypeName
- the name of the solver. Refer to NX help for more informationanalysisTypeType
- the name of the analysis type. Refer to NX help for more informationabstractionType
- the axisymmetric abstraction type. Refer to NX help for more informationdescription
- description
NXException
RemoteException
void finalizeCreation(Part cadPart, String solverTypeName, String analysisTypeType, String[] description) throws NXException, RemoteException
finalizeCreation(nxopen.Part, java.lang.String, java.lang.String, nxopen.cae.BaseFemPart.AxisymAbstractionType, java.lang.String[], boolean, nxopen.CoordinateSystem)
that includes abstraction type instead.
cadPart
- the cad part to be associated with the fem partsolverTypeName
- the name of the solver. Refer to NX help for more informationanalysisTypeType
- the name of the analysis type. Refer to NX help for more informationdescription
- description
NXException
RemoteException
Part masterCadPart() throws NXException, RemoteException
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.