public class SurfaceFinishStandard extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ANSI
ANSI
|
static int |
_DIN
DIN
|
static int |
_DIN2002
DIN 2002
|
static int |
_ESKD
ESKD
|
static int |
_GB
GB131-93
|
static int |
_ISO
ISO
|
static int |
_ISO2002
ISO 2002
|
static int |
_JIS
JIS
|
static SurfaceFinishStandard |
ANSI
ANSI
|
static SurfaceFinishStandard |
DIN
DIN
|
static SurfaceFinishStandard |
DIN2002
DIN 2002
|
static SurfaceFinishStandard |
ESKD
ESKD
|
static SurfaceFinishStandard |
GB
GB131-93
|
static SurfaceFinishStandard |
ISO
ISO
|
static SurfaceFinishStandard |
ISO2002
ISO 2002
|
static SurfaceFinishStandard |
JIS
JIS
|
Modifier and Type | Method and Description |
---|---|
static SurfaceFinishStandard |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SurfaceFinishStandard |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SurfaceFinishStandard[] |
values()
Returns an array that contains the values for this enum.
|
public static final SurfaceFinishStandard ANSI
public static final SurfaceFinishStandard ISO
public static final SurfaceFinishStandard JIS
public static final SurfaceFinishStandard DIN
public static final SurfaceFinishStandard ISO2002
public static final SurfaceFinishStandard DIN2002
public static final SurfaceFinishStandard GB
public static final SurfaceFinishStandard ESKD
public static final int _ANSI
public static final int _ISO
public static final int _JIS
public static final int _DIN
public static final int _ISO2002
public static final int _DIN2002
public static final int _GB
public static final int _ESKD
public static SurfaceFinishStandard valueOf(int value)
public static SurfaceFinishStandard valueOf(String name)
public static SurfaceFinishStandard[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.