public static class SurfaceFinishBuilder.StandardType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ANSI
ANSI
|
static int |
_DIN
DIN
|
static int |
_DIN2002
DIN 2002
|
static int |
_ESKD
ESKD
|
static int |
_GB
GB131-93
|
static int |
_ISO
ISO
|
static int |
_ISO2002
ISO 2002
|
static int |
_JIS
JIS
|
static SurfaceFinishBuilder.StandardType |
ANSI
ANSI
|
static SurfaceFinishBuilder.StandardType |
DIN
DIN
|
static SurfaceFinishBuilder.StandardType |
DIN2002
DIN 2002
|
static SurfaceFinishBuilder.StandardType |
ESKD
ESKD
|
static SurfaceFinishBuilder.StandardType |
GB
GB131-93
|
static SurfaceFinishBuilder.StandardType |
ISO
ISO
|
static SurfaceFinishBuilder.StandardType |
ISO2002
ISO 2002
|
static SurfaceFinishBuilder.StandardType |
JIS
JIS
|
Modifier and Type | Method and Description |
---|---|
static SurfaceFinishBuilder.StandardType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SurfaceFinishBuilder.StandardType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SurfaceFinishBuilder.StandardType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SurfaceFinishBuilder.StandardType ANSI
public static final SurfaceFinishBuilder.StandardType ISO
public static final SurfaceFinishBuilder.StandardType JIS
public static final SurfaceFinishBuilder.StandardType DIN
public static final SurfaceFinishBuilder.StandardType ISO2002
public static final SurfaceFinishBuilder.StandardType DIN2002
public static final SurfaceFinishBuilder.StandardType GB
public static final SurfaceFinishBuilder.StandardType ESKD
public static final int _ANSI
public static final int _ISO
public static final int _JIS
public static final int _DIN
public static final int _ISO2002
public static final int _DIN2002
public static final int _GB
public static final int _ESKD
public static SurfaceFinishBuilder.StandardType valueOf(int value)
public static SurfaceFinishBuilder.StandardType valueOf(String name)
public static SurfaceFinishBuilder.StandardType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.