UserDefinedClass Class¶
-
class
NXOpen.UserDefinedObjects.
UserDefinedClass
¶ Bases:
NXOpen.TransientObject
JA interface for the UserDefinedClass object
To create a new instance of this class, use
NXOpen.UserDefinedObjects.UserDefinedClassManager.NewUserDefinedClass()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AllowOwnedObjectSelectionOption | Returns or sets the allow owned object selection flag. |
AllowQueryClassFromName | Returns or sets the allow query class from name flag. |
ClassName | Returns the class name of the NXOpen.UserDefinedObjects.UserDefinedClass . |
FriendlyName | Returns the friendly name of the NXOpen.UserDefinedObjects.UserDefinedClass . |
WarnUserFlag | Returns or sets the warn user flag. |
Methods¶
Method | Description |
---|---|
AddAttentionPointHandler | Registers the attention point callback. |
AddDeleteHandler | Registers the delete callback. |
AddDisplayHandler | Registers UDO display callback. |
AddEditHandler | Registers the edit callback. |
AddFitHandler | Registers the fit callback. |
AddInformationHandler | Registers the information callback. |
AddScreenSizeFitHandler | Registers the screen size fit callback. |
AddSelectionHandler | Registers the UDO selection callback. |
AddSuppressHandler | Registers the suppress callback. |
AddUpdateHandler | Registers the update callback. |
Dispose | Frees the memory associated with this object. |
GetIsOccurrenceableFlag | Gets the is occurrenceable flag for this class. |
SetIsOccurrenceableFlag | Sets the is occurrenceable flag for this class. |
Enumerations¶
UserDefinedClassAllowOwnedObjectSelection Enumeration | Allow owned object selection on all objects owned by an object of this NXOpen.UserDefinedObjects.UserDefinedClass . |
UserDefinedClassAllowQueryClass Enumeration | Allow query class from name options for a NXOpen.UserDefinedObjects.UserDefinedObject of this class. |
UserDefinedClassSelection Enumeration | Allow query class from name options for a NXOpen.UserDefinedObjects.UserDefinedObject . |
Property Detail¶
AllowOwnedObjectSelectionOption¶
-
UserDefinedClass.
AllowOwnedObjectSelectionOption
¶ Returns or sets the allow owned object selection flag.
Specifies whether or not you have permission to select objects owned by
NXOpen.UserDefinedObjects.UserDefinedObject
‘s of this class.-------------------------------------
Getter Method
Signature
AllowOwnedObjectSelectionOption()
Returns: Return type: NXOpen.UserDefinedObjects.UserDefinedClassAllowOwnedObjectSelection
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllowOwnedObjectSelectionOption(allowOwnedObjectSelectionOption)
Parameters: allowOwnedObjectSelectionOption ( NXOpen.UserDefinedObjects.UserDefinedClassAllowOwnedObjectSelection
) –New in version NX5.0.0.
License requirements: None.
AllowQueryClassFromName¶
-
UserDefinedClass.
AllowQueryClassFromName
¶ Returns or sets the allow query class from name flag.
Specifies whether or not you are allowed to query the
NXOpen.UserDefinedObjects.UserDefinedObject
from the class name.-------------------------------------
Getter Method
Signature
AllowQueryClassFromName()
Returns: Return type: NXOpen.UserDefinedObjects.UserDefinedClassAllowQueryClass
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllowQueryClassFromName(allowQueryClassFromName)
Parameters: allowQueryClassFromName ( NXOpen.UserDefinedObjects.UserDefinedClassAllowQueryClass
) –New in version NX5.0.0.
License requirements: None.
ClassName¶
-
UserDefinedClass.
ClassName
¶ Returns the class name of the
NXOpen.UserDefinedObjects.UserDefinedClass
.-------------------------------------
Getter Method
Signature
ClassName()
Returns: The real class name (non-displayed, non-user-friendly). Return type: str New in version NX5.0.0.
License requirements: None.
FriendlyName¶
-
UserDefinedClass.
FriendlyName
¶ Returns the friendly name of the
NXOpen.UserDefinedObjects.UserDefinedClass
.-------------------------------------
Getter Method
Signature
FriendlyName()
Returns: The Friendly Name is the displayed class name inside of NX. For example, if you select an object in NX and filter by type, this is the name shown for type selection :rtype: str
New in version NX5.0.0.
License requirements: None.
WarnUserFlag¶
-
UserDefinedClass.
WarnUserFlag
¶ Returns or sets the warn user flag.
Specifies the behavior of warning the user if a
NXOpen.UserDefinedObjects.UserDefinedObject
of the givenNXOpen.UserDefinedObjects.UserDefinedClass
is found in a part, but the code implementing the methods for the UDO is not loaded. The default action is to not warn the user. If the UDO author sets this flag to TRUE, all UDO’s of this class that are created will be marked so that the user will be warned if the UDO methods have not been loaded, but a UDO of the class is in the part. This warning will be issued to the listing window, when the first object of the given class is retrieved. This warning will only be given once per session.This flag is set on every UDO object. Therefore for any part, there may be a mixture UDO objects of a given class, some having this flag set to TRUE and some objects having the flag set to FALSE. This is particularly true since all UDO objects created before NX 3.0 will have this flag set to FALSE. If the UDO methods for a class are not loaded, any one UDO with this flag set to TRUE in a part is enough for the warning to be issued to the listing window.
-------------------------------------
Getter Method
Signature
WarnUserFlag()
Returns: TRUE - the user will be warned when opening a part containing a UDO of this class without first loading it’s required methods. FALSE - the user will NOT be warned. Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WarnUserFlag(warnUser)
Parameters: warnUser (bool) – TRUE - the user will be warned when opening a part containing a UDO of this class without first loading it’s required methods. FALSE - the user will NOT be warned. New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddAttentionPointHandler¶
-
UserDefinedClass.
AddAttentionPointHandler
¶ Registers the attention point callback.
Signature
AddAttentionPointHandler(displayEvent)
Parameters: displayEvent (CallableObject) – New in version NX5.0.0.
License requirements: None.
AddDeleteHandler¶
-
UserDefinedClass.
AddDeleteHandler
¶ Registers the delete callback.
Signature
AddDeleteHandler(linkEvent)
Parameters: linkEvent (CallableObject) – New in version NX5.0.0.
License requirements: None.
AddDisplayHandler¶
-
UserDefinedClass.
AddDisplayHandler
¶ Registers UDO display callback.
Signature
AddDisplayHandler(displayEvent)
Parameters: displayEvent (CallableObject) – New in version NX5.0.0.
License requirements: None.
AddEditHandler¶
-
UserDefinedClass.
AddEditHandler
¶ Registers the edit callback.
Signature
AddEditHandler(udoEvent)
Parameters: udoEvent (CallableObject) – New in version NX5.0.0.
License requirements: None.
AddFitHandler¶
-
UserDefinedClass.
AddFitHandler
¶ Registers the fit callback.
Signature
AddFitHandler(displayEvent)
Parameters: displayEvent (CallableObject) – New in version NX5.0.0.
License requirements: None.
AddInformationHandler¶
-
UserDefinedClass.
AddInformationHandler
¶ Registers the information callback.
Signature
AddInformationHandler(udoEvent)
Parameters: udoEvent (CallableObject) – New in version NX5.0.0.
License requirements: None.
AddScreenSizeFitHandler¶
-
UserDefinedClass.
AddScreenSizeFitHandler
¶ Registers the screen size fit callback.
The screen size fit callback is called when it is necesary to determine the bounding box of a screen size object (one which remains the same size on the screen independent of the view scale) during a fit computation. As of NX 8.0 the only geometry types supported for User Defined Objects which are screen size are ScreenStandardText and AbsoluteRotationScreenSizeText. If your User Defined Object does not have any of these objects, then you should not call
NXOpen.UserDefinedObjects.UserDefinedClass.AddScreenSizeFitHandler()
because to do do would incur a performance penalty.Signature
AddScreenSizeFitHandler(displayEvent)
Parameters: displayEvent (CallableObject) – New in version NX8.0.0.
License requirements: None.
AddSelectionHandler¶
-
UserDefinedClass.
AddSelectionHandler
¶ Registers the UDO selection callback.
Signature
AddSelectionHandler(displayEvent)
Parameters: displayEvent (CallableObject) – New in version NX5.0.0.
License requirements: None.
AddSuppressHandler¶
-
UserDefinedClass.
AddSuppressHandler
¶ Registers the suppress callback.
Note this callback is not called unless you have a UDO FEATURE. Also it may not get called when the system automatically suppresses the feature during update.
Also note the user should check the suppression status of the feature in their callback to see if the input udo feature is currently getting suppressed or unsuppressed.
Signature
AddSuppressHandler(udoEvent)
Parameters: udoEvent (CallableObject) – New in version NX5.0.0.
License requirements: None.
AddUpdateHandler¶
-
UserDefinedClass.
AddUpdateHandler
¶ Registers the update callback.
Signature
AddUpdateHandler(linkEvent)
Parameters: linkEvent (CallableObject) – New in version NX5.0.0.
License requirements: None.
Dispose¶
-
UserDefinedClass.
Dispose
¶ Frees the memory associated with this object.
After invocation of this method, the object is no longer valid.
Signature
Dispose()
New in version NX5.0.0.
License requirements: None.
GetIsOccurrenceableFlag¶
-
UserDefinedClass.
GetIsOccurrenceableFlag
¶ Gets the is occurrenceable flag for this class.
Legacy Open C UDO’s required a reference UDO to determine Occurrenceability. Occurrenceability is now set on a class by class basis (no reference UDO required). In the event that you have a legacy UDO you wish to query for occurenceability, you will need set the is occurrenceable flag with the new native language method (which does not require a reference UDO) If you do not set the is occurrenceable flag, and instead use the old open c is occurrenceable callback, you will risk error raising during this method because we will automatically pass None in as the reference UDO to the legacy is occurrenceable callback.
Signature
GetIsOccurrenceableFlag()
Returns: Specifies whether or not to populate occurrences for NXOpen.UserDefinedObjects.UserDefinedObject
‘s of this class.Return type: bool New in version NX5.0.0.
License requirements: None.
SetIsOccurrenceableFlag¶
-
UserDefinedClass.
SetIsOccurrenceableFlag
¶ Sets the is occurrenceable flag for this class.
Signature
SetIsOccurrenceableFlag(isOccurrenceable)
Parameters: isOccurrenceable (bool) – Specifies whether or not to populate occurrences for NXOpen.UserDefinedObjects.UserDefinedObject
‘s of this class.New in version NX5.0.0.
License requirements: None.