UserDefinedClassAllowQueryClass Enumeration

NXOpen.UserDefinedObjects.UserDefinedClass.AllowQueryClass is an alias for NXOpen.UserDefinedObjects.UserDefinedClassAllowQueryClass

class NXOpen.UserDefinedObjects.UserDefinedClassAllowQueryClass

Bases: object

Allow query class from name options for a NXOpen.UserDefinedObjects.UserDefinedObject of this class.

Enum Members

Enum Member Enum Member Description
Off
You do NOT have permission to query the class from it’s name.
On
You have permission to query the class from it’s name.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.