UserDefinedClassSelection Enumeration

NXOpen.UserDefinedObjects.UserDefinedClass.Selection is an alias for NXOpen.UserDefinedObjects.UserDefinedClassSelection

class NXOpen.UserDefinedObjects.UserDefinedClassSelection

Bases: object

Allow query class from name options for a NXOpen.UserDefinedObjects.UserDefinedObject.

Enum Members

Enum Member Enum Member Description
Off
UDO’s of this class will NOT be selectable.
On
UDO’s of this class will be selectable.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.