GuidedExtensionBuilder Class¶
-
class
NXOpen.Tooling.
GuidedExtensionBuilder
¶ Bases:
NXOpen.Builder
Builder for creating Guided Extension surface in NX
To create a new instance of this class, use
NXOpen.Tooling.GuidedExtensionManager.CreateBuilder()
Default values.
Property Value AngleTolerance 0.5 CheckSurfaces 0 DistanceTolerance 0.01 ExtendLength.Value 10 (millimeters part), 10 (inches part) GuideLineAngle1.Value 0 GuideLineAngle2.Value 0 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance for use in creating the guided extension surfaces |
CheckSurfaces | Returns or sets the option for checking the resulting guided extension surfaces for geometry issues |
DistanceTolerance | Returns or sets the distance tolerance for use in creating the guided extension surfaces |
ExtendLength | Returns the extend length for use in creating the guided extension surfaces |
GuideLineAngle1 | Returns the rotation angle for the first guide line at one of the end points of the selected segment |
GuideLineAngle2 | Returns the rotation angle for the second guide line at one of the end points of the selected segment |
SegmentEdges | Returns the list of segment edges that represent a segment |
SheetEdges | Returns the sheet edges of a sheet body |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ChangeGuideLineDirectionAndLength | Changes the direction and length of a guide line. |
Commit | Commits any edits that have been applied to the builder. |
CreateGuideLine | Creates a guide line at one of the end points of the sheet edge in the selection. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
MergeSegment | Merges the selected segment with its neighboring segments. |
ResetAllSegments | The action that resets all the segments in the loop to their original state |
RestoreSegments | Unmerges the selected segment restoring the original segments before the merge using Tooling.GuidedExtensionBuilder.MergeSegment() . |
SetLastSelectedLoopIndex | Sets the loop index for the last selected loop which contains the last selected edge. |
SetReverseExtendDirection | Reverses surface extend direction |
SetSelectedSegmentType | Sets the segment type for the selected segment. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
SplitSegment | Splits the selected segment into multiple segments by placing guide lines at end points of the edges for the selected segment. |
UpdateAllGuideLinesLength | Updates the length of all the guide lines whenever the user changes the extend length of the surfaces interactively. |
UpdateSheetEdges | Updates the information for the sheet edges of the selected section whenever sheet edges are selected or de-selected. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GuidedExtensionBuilderSegmentType Enumeration | Segment type for segments |
Property Detail¶
AngleTolerance¶
-
GuidedExtensionBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance for use in creating the guided extension surfaces
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
AngleTolerance(angleTolerance)
Parameters: angleTolerance (float) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
CheckSurfaces¶
-
GuidedExtensionBuilder.
CheckSurfaces
¶ Returns or sets the option for checking the resulting guided extension surfaces for geometry issues
-------------------------------------
Getter Method
Signature
CheckSurfaces()
Returns: Return type: bool New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
CheckSurfaces(checkSurfaces)
Parameters: checkSurfaces (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
DistanceTolerance¶
-
GuidedExtensionBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance for use in creating the guided extension surfaces
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
ExtendLength¶
-
GuidedExtensionBuilder.
ExtendLength
¶ Returns the extend length for use in creating the guided extension surfaces
-------------------------------------
Getter Method
Signature
ExtendLength()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
GuideLineAngle1¶
-
GuidedExtensionBuilder.
GuideLineAngle1
¶ Returns the rotation angle for the first guide line at one of the end points of the selected segment
-------------------------------------
Getter Method
Signature
GuideLineAngle1()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
GuideLineAngle2¶
-
GuidedExtensionBuilder.
GuideLineAngle2
¶ Returns the rotation angle for the second guide line at one of the end points of the selected segment
-------------------------------------
Getter Method
Signature
GuideLineAngle2()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
SegmentEdges¶
-
GuidedExtensionBuilder.
SegmentEdges
¶ Returns the list of segment edges that represent a segment
-------------------------------------
Getter Method
Signature
SegmentEdges()
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
SheetEdges¶
-
GuidedExtensionBuilder.
SheetEdges
¶ Returns the sheet edges of a sheet body
-------------------------------------
Getter Method
Signature
SheetEdges()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
Method Detail¶
ChangeGuideLineDirectionAndLength¶
-
GuidedExtensionBuilder.
ChangeGuideLineDirectionAndLength
¶ Changes the direction and length of a guide line.
Signature
ChangeGuideLineDirectionAndLength(guideLine, guideLineVector, guideLineLength)
Parameters: - guideLine (
NXOpen.Curve
) – Guide line to be changed - guideLineVector (
NXOpen.Vector3d
) – Direction vector - guideLineLength (float) – Length of guide line
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
- guideLine (
CreateGuideLine¶
-
GuidedExtensionBuilder.
CreateGuideLine
¶ Creates a guide line at one of the end points of the sheet edge in the selection.
Signature
CreateGuideLine(assocEdge, guideLinePnt, guideLineVector, guideLineLength)
Parameters: - assocEdge (
NXOpen.Edge
) – Associated curve of the guide line to be created - guideLinePnt (
NXOpen.Point3d
) – Guide line point - guideLineVector (
NXOpen.Vector3d
) – Guide line vector - guideLineLength (float) – Guide line length
Returns: Guide line created
Return type: New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
- assocEdge (
MergeSegment¶
-
GuidedExtensionBuilder.
MergeSegment
¶ Merges the selected segment with its neighboring segments.
Signature
MergeSegment()
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
ResetAllSegments¶
-
GuidedExtensionBuilder.
ResetAllSegments
¶ The action that resets all the segments in the loop to their original state
Signature
ResetAllSegments()
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
RestoreSegments¶
-
GuidedExtensionBuilder.
RestoreSegments
¶ Unmerges the selected segment restoring the original segments before the merge using
Tooling.GuidedExtensionBuilder.MergeSegment()
.Signature
RestoreSegments()
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
SetLastSelectedLoopIndex¶
-
GuidedExtensionBuilder.
SetLastSelectedLoopIndex
¶ Sets the loop index for the last selected loop which contains the last selected edge.
Signature
SetLastSelectedLoopIndex(lastSelectedLoopIndex)
Parameters: lastSelectedLoopIndex (int) – Loop index of the last selected loop New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
SetReverseExtendDirection¶
-
GuidedExtensionBuilder.
SetReverseExtendDirection
¶ Reverses surface extend direction
Signature
SetReverseExtendDirection(reverseExtendDirection)
Parameters: reverseExtendDirection (bool) – Reverse surface extend direction New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
SetSelectedSegmentType¶
-
GuidedExtensionBuilder.
SetSelectedSegmentType
¶ Sets the segment type for the selected segment.
Signature
SetSelectedSegmentType(segmentType)
Parameters: segmentType ( NXOpen.Tooling.GuidedExtensionBuilderSegmentType
) – Segment type for the selected segmentNew in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
SplitSegment¶
-
GuidedExtensionBuilder.
SplitSegment
¶ Splits the selected segment into multiple segments by placing guide lines at end points of the edges for the selected segment.
Signature
SplitSegment()
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
UpdateAllGuideLinesLength¶
-
GuidedExtensionBuilder.
UpdateAllGuideLinesLength
¶ Updates the length of all the guide lines whenever the user changes the extend length of the surfaces interactively.
Signature
UpdateAllGuideLinesLength()
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
UpdateSheetEdges¶
-
GuidedExtensionBuilder.
UpdateSheetEdges
¶ Updates the information for the sheet edges of the selected section whenever sheet edges are selected or de-selected.
Signature
UpdateSheetEdges()
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR nx_freeform_2 (“advanced freeform modeling”) OR ug_mold_design (“UG MOLD”) OR die_engineering (“DIE ENGINEERING”)
Validate¶
-
GuidedExtensionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.