GuidedExtensionBuilderSegmentType Enumeration

NXOpen.Tooling.GuidedExtensionBuilder.SegmentType is an alias for NXOpen.Tooling.GuidedExtensionBuilderSegmentType

class NXOpen.Tooling.GuidedExtensionBuilderSegmentType

Bases: object

Segment type for segments

Enum Members

Enum Member Enum Member Description
Normal
Normal segment type
Transition
Transition segment type
Bypass
Bypass segment type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.