ElectrodeBlankBuilder Class¶
-
class
NXOpen.Tooling.
ElectrodeBlankBuilder
¶ Bases:
NXOpen.Builder
Design electrode blank builder to create an electrode blank for the selected body.
To create a new instance of this class, use
NXOpen.Tooling.ElectrodeDesignCollection.CreateBlankBuilder()
Default values.
Property Value Angle.Value 0 BlendRadius.Value 0 (millimeters part), 0 (inches part) ExtensionHeight.Value 5 (millimeters part), 0.2 (inches part) JointMethod Extrude KeepSize 0 KeepZValueInSameMSet 0 Material Copper ReferencePointPrecision 1 Rename 0 RotationAngle.Value 0 RoundCrossLinesPosition 0 Shape Block UniteBodies 1 XRefValue.Value 0 (millimeters part), 0 (inches part) YRefValue.Value 0 (millimeters part), 0 (inches part) ZRefValue.Value 0 (millimeters part), 0 (inches part) New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the angle of the joint object. |
Blank | Returns the blank to be edited. |
BlankMatrix | Returns or sets the blank matrix. |
BlendRadius | Returns the default blend radius of blended edges. |
CrossLinesRatio | Returns or sets the ratio of cross center lines. |
ExtensionHeight | Returns the default extension height between head bodies and the blank. |
HeadBodies | Returns the head bodies to be used to create a blank. |
JointFace | Returns the face to create a joint object between the blank and head bodies. |
JointMethod | Returns or sets the joint object type. |
KeepSize | Returns or sets the option to keep size of the blank or not. |
KeepZValueInSameMSet | Returns or sets the option to specify whether to keep the Z values of all blanks in the current machine set CSYS. |
Material | Returns or sets the material of the blank. |
MsetPart | Returns or sets the current machine set under which a blank is added. |
MultiPositionBuilder | Returns or sets the multi position builder. |
ReferenceCenter | Returns or sets the blank reference point. |
ReferencePointPrecision | Returns or sets the precision of the reference coordinates in the machine set csys. |
Rename | Returns or sets the option to use the part name management dialog box or not. |
ReusablePartBuilder | Returns or sets the reusable part builder. |
RotationAngle | Returns the rotation angle of blank. |
RoundCrossLinesPosition | Returns or sets the option to round the position of cross lines or not. |
Shape | Returns or sets the shape of the blank. |
Tag | Returns the Tag for this object. |
UniteBodies | Returns or sets the option to unite head bodies, the extension and the blank or not. |
XRefValue | Returns the X value of the blank origin in the current machine set coordinator. |
YRefValue | Returns the Y value of the blank origin in the current machine set coordinator. |
ZRefValue | Returns the Z value of the blank origin in the current machine set coordinator. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ElectrodeBlankBuilderBlankMaterial Enumeration | Represents the blank material option. |
ElectrodeBlankBuilderBlankShape Enumeration | Represents the electrode blank shape option. |
ElectrodeBlankBuilderJointObject Enumeration | Represents the transition type between head bodies and the blank. |
Property Detail¶
Angle¶
-
ElectrodeBlankBuilder.
Angle
¶ Returns the angle of the joint object.
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Blank¶
-
ElectrodeBlankBuilder.
Blank
¶ Returns the blank to be edited.
-------------------------------------
Getter Method
Signature
Blank()
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX8.0.0.
License requirements: None.
BlankMatrix¶
-
ElectrodeBlankBuilder.
BlankMatrix
¶ Returns or sets the blank matrix.
-------------------------------------
Getter Method
Signature
BlankMatrix()
Returns: blank matrix Return type: NXOpen.Matrix3x3
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlankMatrix(matrix)
Parameters: matrix ( NXOpen.Matrix3x3
) – blank matrixNew in version NX8.5.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
BlendRadius¶
-
ElectrodeBlankBuilder.
BlendRadius
¶ Returns the default blend radius of blended edges.
-------------------------------------
Getter Method
Signature
BlendRadius()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
CrossLinesRatio¶
-
ElectrodeBlankBuilder.
CrossLinesRatio
¶ Returns or sets the ratio of cross center lines.
-------------------------------------
Getter Method
Signature
CrossLinesRatio()
Returns: ratio Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CrossLinesRatio(ratio)
Parameters: ratio (float) – ratio New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
ExtensionHeight¶
-
ElectrodeBlankBuilder.
ExtensionHeight
¶ Returns the default extension height between head bodies and the blank.
-------------------------------------
Getter Method
Signature
ExtensionHeight()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
HeadBodies¶
-
ElectrodeBlankBuilder.
HeadBodies
¶ Returns the head bodies to be used to create a blank.
-------------------------------------
Getter Method
Signature
HeadBodies()
Returns: Return type: NXOpen.SelectBodyList
New in version NX8.0.0.
License requirements: None.
JointFace¶
-
ElectrodeBlankBuilder.
JointFace
¶ Returns the face to create a joint object between the blank and head bodies.
-------------------------------------
Getter Method
Signature
JointFace()
Returns: Return type: NXOpen.SelectFace
New in version NX8.0.0.
License requirements: None.
JointMethod¶
-
ElectrodeBlankBuilder.
JointMethod
¶ Returns or sets the joint object type.
-------------------------------------
Getter Method
Signature
JointMethod()
Returns: Return type: NXOpen.Tooling.ElectrodeBlankBuilderJointObject
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
JointMethod(jointMethod)
Parameters: jointMethod ( NXOpen.Tooling.ElectrodeBlankBuilderJointObject
) –New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
KeepSize¶
-
ElectrodeBlankBuilder.
KeepSize
¶ Returns or sets the option to keep size of the blank or not.
-------------------------------------
Getter Method
Signature
KeepSize()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepSize(keepSize)
Parameters: keepSize (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
KeepZValueInSameMSet¶
-
ElectrodeBlankBuilder.
KeepZValueInSameMSet
¶ Returns or sets the option to specify whether to keep the Z values of all blanks in the current machine set CSYS.
-------------------------------------
Getter Method
Signature
KeepZValueInSameMSet()
Returns: keep z value in machine set or not Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepZValueInSameMSet(keepValue)
Parameters: keepValue (bool) – keep z value in machine set or not New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Material¶
-
ElectrodeBlankBuilder.
Material
¶ Returns or sets the material of the blank.
-------------------------------------
Getter Method
Signature
Material()
Returns: Return type: NXOpen.Tooling.ElectrodeBlankBuilderBlankMaterial
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Material(material)
Parameters: material ( NXOpen.Tooling.ElectrodeBlankBuilderBlankMaterial
) –New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
MsetPart¶
-
ElectrodeBlankBuilder.
MsetPart
¶ Returns or sets the current machine set under which a blank is added.
-------------------------------------
Getter Method
Signature
MsetPart()
Returns: the machine set part Return type: NXOpen.TaggedObject
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MsetPart(mset)
Parameters: mset ( NXOpen.TaggedObject
) – the machine set partNew in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
MultiPositionBuilder¶
-
ElectrodeBlankBuilder.
MultiPositionBuilder
¶ Returns or sets the multi position builder.
-------------------------------------
Getter Method
Signature
MultiPositionBuilder()
Returns: multi position builder tag Return type: NXOpen.TaggedObject
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MultiPositionBuilder(builderTag)
Parameters: builderTag ( NXOpen.TaggedObject
) – multi position builder tagNew in version NX8.5.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
ReferenceCenter¶
-
ElectrodeBlankBuilder.
ReferenceCenter
¶ Returns or sets the blank reference point.
-------------------------------------
Getter Method
Signature
ReferenceCenter()
Returns: blank position Return type: NXOpen.Point3d
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceCenter(point)
Parameters: point ( NXOpen.Point3d
) – blank positionNew in version NX8.5.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
ReferencePointPrecision¶
-
ElectrodeBlankBuilder.
ReferencePointPrecision
¶ Returns or sets the precision of the reference coordinates in the machine set csys.
-------------------------------------
Getter Method
Signature
ReferencePointPrecision()
Returns: precision value Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferencePointPrecision(precision)
Parameters: precision (float) – precision value New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Rename¶
-
ElectrodeBlankBuilder.
Rename
¶ Returns or sets the option to use the part name management dialog box or not.
-------------------------------------
Getter Method
Signature
Rename()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Rename(rename)
Parameters: rename (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
ReusablePartBuilder¶
-
ElectrodeBlankBuilder.
ReusablePartBuilder
¶ Returns or sets the reusable part builder.
-------------------------------------
Getter Method
Signature
ReusablePartBuilder()
Returns: reusable part builder tag Return type: NXOpen.TaggedObject
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReusablePartBuilder(builderTag)
Parameters: builderTag ( NXOpen.TaggedObject
) – reusable part builder tagNew in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
RotationAngle¶
-
ElectrodeBlankBuilder.
RotationAngle
¶ Returns the rotation angle of blank.
-------------------------------------
Getter Method
Signature
RotationAngle()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RoundCrossLinesPosition¶
-
ElectrodeBlankBuilder.
RoundCrossLinesPosition
¶ Returns or sets the option to round the position of cross lines or not.
-------------------------------------
Getter Method
Signature
RoundCrossLinesPosition()
Returns: round cross lines or not Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RoundCrossLinesPosition(round)
Parameters: round (bool) – round cross lines or not New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Shape¶
-
ElectrodeBlankBuilder.
Shape
¶ Returns or sets the shape of the blank.
-------------------------------------
Getter Method
Signature
Shape()
Returns: Return type: NXOpen.Tooling.ElectrodeBlankBuilderBlankShape
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Shape(shape)
Parameters: shape ( NXOpen.Tooling.ElectrodeBlankBuilderBlankShape
) –New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
UniteBodies¶
-
ElectrodeBlankBuilder.
UniteBodies
¶ Returns or sets the option to unite head bodies, the extension and the blank or not.
-------------------------------------
Getter Method
Signature
UniteBodies()
Returns: unite head, extension and blank together or not Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UniteBodies(unite)
Parameters: unite (bool) – unite head, extension and blank together or not New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
XRefValue¶
-
ElectrodeBlankBuilder.
XRefValue
¶ Returns the X value of the blank origin in the current machine set coordinator.
-------------------------------------
Getter Method
Signature
XRefValue()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
YRefValue¶
-
ElectrodeBlankBuilder.
YRefValue
¶ Returns the Y value of the blank origin in the current machine set coordinator.
-------------------------------------
Getter Method
Signature
YRefValue()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ZRefValue¶
-
ElectrodeBlankBuilder.
ZRefValue
¶ Returns the Z value of the blank origin in the current machine set coordinator.
-------------------------------------
Getter Method
Signature
ZRefValue()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ElectrodeBlankBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.