ElectrodeBlankBuilderJointObject Enumeration¶
NXOpen.Tooling.ElectrodeBlankBuilder.JointObject is an alias for NXOpen.Tooling.ElectrodeBlankBuilderJointObject
-
class
NXOpen.Tooling.
ElectrodeBlankBuilderJointObject
¶ Bases:
object
Represents the transition type between head bodies and the blank.
Enum Members
Enum Member Enum Member Description Extrude extrude body from joint face to blankOffset create offset feature from joint face to blankNotSet nothing to do-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-