ElectrodeBlankBuilderBlankMaterial Enumeration

NXOpen.Tooling.ElectrodeBlankBuilder.BlankMaterial is an alias for NXOpen.Tooling.ElectrodeBlankBuilderBlankMaterial

class NXOpen.Tooling.ElectrodeBlankBuilderBlankMaterial

Bases: object

Represents the blank material option.

Enum Members

Enum Member Enum Member Description
Copper
the material of the blank is copper
Graphite
the material of the blank is graphite
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.