EWDraftingBuilder Class¶
-
class
NXOpen.Tooling.
EWDraftingBuilder
¶ Bases:
NXOpen.Builder
Represents the drafting builder which is used to create electrode drafting.
To create a new instance of this class, use
NXOpen.Tooling.ElectrodeDesignCollection.CreateEwdraftingBuilder()
Default values.
Property Value CncOption 0 CncTemplate CncTemplate1 DraftingMode Create DrawingType MasterModel EdmOption 1 EdmTemplate EdmTemplate1 IncludeOption 1 OutputPDF 0 OutputSameSheet 0 RenameComponent 0 SheetName Sh1 UseInstance 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
BlankComps | Returns the blank components used to create drafting. |
CncOption | Returns or sets the option to create cnc sheet type drafting or not. |
CncTemplate | Returns or sets the template of cnc sheet type to create drafting. |
DraftingMode | Returns or sets the drafting mode: create, add or edit. |
DrawingType | Returns or sets the drawing type used to create drafting. |
EdmOption | Returns or sets the option to create edm sheet type drafting or not. |
EdmTemplate | Returns or sets the template of edm sheet type to create drafting. |
IncludeFixture | Returns or sets the option used to include fixture when creating drafting. |
IncludeOption | Returns or sets the option used to include the working component when creating drafting. |
MasterModelCncPartName | Returns or sets the name to create a master model part for CNC drawing. |
MasterModelEdmPartName | Returns or sets the name to create a master model part for EDM drawing. |
NameRule | Returns or sets the name rule used to create drafting part. |
OutputPDF | Returns or sets the option used to output pdf file when creating drafting. |
OutputSameSheet | Returns or sets the option used to output all the blanks in the same sheet. |
RenameComponent | Returns or sets the option used to rename the part which is created. |
SheetName | Returns or sets the sheet name option used to edit drafting. |
Tag | Returns the Tag for this object. |
UseInstance | Returns or sets the option used to display and use instance of electrode to create drawing. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
EWDraftingBuilderCNCTemplateOption Enumeration | the template option of cnc sheet type |
EWDraftingBuilderDrawingOption Enumeration | the drawing type |
EWDraftingBuilderEDMTemplateOption Enumeration | the template option of edm sheet type |
EWDraftingBuilderModeOption Enumeration | the drafting mode option |
EWDraftingBuilderNameOption Enumeration | the drawing sheet name option |
Property Detail¶
BlankComps¶
-
EWDraftingBuilder.
BlankComps
¶ Returns the blank components used to create drafting.
-------------------------------------
Getter Method
Signature
BlankComps()
Returns: Return type: NXOpen.SelectPartList
New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
CncOption¶
-
EWDraftingBuilder.
CncOption
¶ Returns or sets the option to create cnc sheet type drafting or not.
-------------------------------------
Getter Method
Signature
CncOption()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
CncOption(cncOption)
Parameters: cncOption (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
CncTemplate¶
-
EWDraftingBuilder.
CncTemplate
¶ Returns or sets the template of cnc sheet type to create drafting.
-------------------------------------
Getter Method
Signature
CncTemplate()
Returns: Return type: NXOpen.Tooling.EWDraftingBuilderCNCTemplateOption
New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
CncTemplate(cncTemplate)
Parameters: cncTemplate ( NXOpen.Tooling.EWDraftingBuilderCNCTemplateOption
) –New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
DraftingMode¶
-
EWDraftingBuilder.
DraftingMode
¶ Returns or sets the drafting mode: create, add or edit.
-------------------------------------
Getter Method
Signature
DraftingMode()
Returns: Return type: NXOpen.Tooling.EWDraftingBuilderModeOption
New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
DraftingMode(draftingMode)
Parameters: draftingMode ( NXOpen.Tooling.EWDraftingBuilderModeOption
) –New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
DrawingType¶
-
EWDraftingBuilder.
DrawingType
¶ Returns or sets the drawing type used to create drafting.
-------------------------------------
Getter Method
Signature
DrawingType()
Returns: Return type: NXOpen.Tooling.EWDraftingBuilderDrawingOption
New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
DrawingType(drawingType)
Parameters: drawingType ( NXOpen.Tooling.EWDraftingBuilderDrawingOption
) –New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
EdmOption¶
-
EWDraftingBuilder.
EdmOption
¶ Returns or sets the option to create edm sheet type drafting or not.
-------------------------------------
Getter Method
Signature
EdmOption()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
EdmOption(edmOption)
Parameters: edmOption (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
EdmTemplate¶
-
EWDraftingBuilder.
EdmTemplate
¶ Returns or sets the template of edm sheet type to create drafting.
-------------------------------------
Getter Method
Signature
EdmTemplate()
Returns: Return type: NXOpen.Tooling.EWDraftingBuilderEDMTemplateOption
New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
EdmTemplate(edmTemplate)
Parameters: edmTemplate ( NXOpen.Tooling.EWDraftingBuilderEDMTemplateOption
) –New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
IncludeFixture¶
-
EWDraftingBuilder.
IncludeFixture
¶ Returns or sets the option used to include fixture when creating drafting.
-------------------------------------
Getter Method
Signature
IncludeFixture()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
IncludeFixture(includeFixture)
Parameters: includeFixture (bool) – New in version NX10.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
IncludeOption¶
-
EWDraftingBuilder.
IncludeOption
¶ Returns or sets the option used to include the working component when creating drafting.
-------------------------------------
Getter Method
Signature
IncludeOption()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
IncludeOption(includeOption)
Parameters: includeOption (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
MasterModelCncPartName¶
-
EWDraftingBuilder.
MasterModelCncPartName
¶ Returns or sets the name to create a master model part for CNC drawing.
-------------------------------------
Getter Method
Signature
MasterModelCncPartName()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MasterModelCncPartName(masterModelPartName)
Parameters: masterModelPartName (str) – New in version NX10.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
MasterModelEdmPartName¶
-
EWDraftingBuilder.
MasterModelEdmPartName
¶ Returns or sets the name to create a master model part for EDM drawing.
-------------------------------------
Getter Method
Signature
MasterModelEdmPartName()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MasterModelEdmPartName(masterModelPartName)
Parameters: masterModelPartName (str) – New in version NX10.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
NameRule¶
-
EWDraftingBuilder.
NameRule
¶ Returns or sets the name rule used to create drafting part.
-------------------------------------
Getter Method
Signature
NameRule()
Returns: Return type: str New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
NameRule(nameRule)
Parameters: nameRule (str) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
OutputPDF¶
-
EWDraftingBuilder.
OutputPDF
¶ Returns or sets the option used to output pdf file when creating drafting.
-------------------------------------
Getter Method
Signature
OutputPDF()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
OutputPDF(outputPDF)
Parameters: outputPDF (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
OutputSameSheet¶
-
EWDraftingBuilder.
OutputSameSheet
¶ Returns or sets the option used to output all the blanks in the same sheet.
-------------------------------------
Getter Method
Signature
OutputSameSheet()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
OutputSameSheet(outputSameSheet)
Parameters: outputSameSheet (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
RenameComponent¶
-
EWDraftingBuilder.
RenameComponent
¶ Returns or sets the option used to rename the part which is created.
-------------------------------------
Getter Method
Signature
RenameComponent()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
RenameComponent(renameComponent)
Parameters: renameComponent (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
SheetName¶
-
EWDraftingBuilder.
SheetName
¶ Returns or sets the sheet name option used to edit drafting.
-------------------------------------
Getter Method
Signature
SheetName()
Returns: Return type: NXOpen.Tooling.EWDraftingBuilderNameOption
New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
SheetName(sheetName)
Parameters: sheetName ( NXOpen.Tooling.EWDraftingBuilderNameOption
) –New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
UseInstance¶
-
EWDraftingBuilder.
UseInstance
¶ Returns or sets the option used to display and use instance of electrode to create drawing.
-------------------------------------
Getter Method
Signature
UseInstance()
Returns: Return type: bool New in version NX9.0.2.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
UseInstance(useInstance)
Parameters: useInstance (bool) – New in version NX9.0.2.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Method Detail¶
Validate¶
-
EWDraftingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.