EWDraftingBuilderDrawingOption Enumeration

NXOpen.Tooling.EWDraftingBuilder.DrawingOption is an alias for NXOpen.Tooling.EWDraftingBuilderDrawingOption

class NXOpen.Tooling.EWDraftingBuilderDrawingOption

Bases: object

the drawing type

Enum Members

Enum Member Enum Member Description
MasterModel
master model
SelfContained
self contained
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.