EWDraftingBuilderCNCTemplateOption Enumeration

NXOpen.Tooling.EWDraftingBuilder.CNCTemplateOption is an alias for NXOpen.Tooling.EWDraftingBuilderCNCTemplateOption

class NXOpen.Tooling.EWDraftingBuilderCNCTemplateOption

Bases: object

the template option of cnc sheet type

Enum Members

Enum Member Enum Member Description
CncTemplate1
template1
CncTemplate2
template2
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.