AddReusableFeatureBuilder Class¶
-
class
NXOpen.Tooling.
AddReusableFeatureBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.AddReusableFeatureBuilder
To create a new instance of this class, use
NXOpen.Tooling.AddReusableFeatureCollection.CreateBuilder()
Default values.
Property Value LayerOption Work SpecifiedLayer 1 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
LayerOption | Returns or sets the layer option |
SpecifiedLayer | Returns or sets the specified layer |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCopyPasteBuilder | Returns the copy paste builder @return |
GetObject | Returns the object currently being edited by this builder. |
GetUserExpressions | Gets the user expressions value |
SetUserExpressions | Sets the user expressions value |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AddReusableFeatureBuilderLayerOptionType Enumeration | Represents the layer option type |
Property Detail¶
LayerOption¶
-
AddReusableFeatureBuilder.
LayerOption
¶ Returns or sets the layer option
-------------------------------------
Getter Method
Signature
LayerOption()
Returns: Return type: NXOpen.Tooling.AddReusableFeatureBuilderLayerOptionType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LayerOption(layerOption)
Parameters: layerOption ( NXOpen.Tooling.AddReusableFeatureBuilderLayerOptionType
) –New in version NX7.5.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SpecifiedLayer¶
-
AddReusableFeatureBuilder.
SpecifiedLayer
¶ Returns or sets the specified layer
-------------------------------------
Getter Method
Signature
SpecifiedLayer()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpecifiedLayer(specifiedLayer)
Parameters: specifiedLayer (int) – New in version NX7.5.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Method Detail¶
GetCopyPasteBuilder¶
-
AddReusableFeatureBuilder.
GetCopyPasteBuilder
¶ Returns the copy paste builder
Signature
GetCopyPasteBuilder()
Returns: Return type: NXOpen.Features.CopyPasteBuilder
New in version NX7.5.0.
License requirements: None.
GetUserExpressions¶
-
AddReusableFeatureBuilder.
GetUserExpressions
¶ Gets the user expressions value
Signature
GetUserExpressions()
Returns: a tuple Return type: A tuple consisting of (userExpressionsName, userExpressionsValue). userExpressionsName is a list of str. User expressions Name userExpressionsValue is a list of str. User expressions Value New in version NX7.5.0.
License requirements: None.
SetUserExpressions¶
-
AddReusableFeatureBuilder.
SetUserExpressions
¶ Sets the user expressions value
Signature
SetUserExpressions(userExpressionsName, userExpressionsValue)
Parameters: - userExpressionsName (list of str) – User expressions Name
- userExpressionsValue (list of str) – User expressions Value
New in version NX7.5.0.
License requirements: None.
Validate¶
-
AddReusableFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.