AddReusableFeatureCollection Class

class NXOpen.Tooling.AddReusableFeatureCollection

Bases: object

Represents a collection of AddReusableFeature

To obtain an instance of this class, refer to NXOpen.Tooling.ToolingManager

New in version NX7.5.0.

Methods

Method Description
CreateBuilder Creates a AddReusableFeature builder @return Add Reusable Feature Builder

Structs

AddReusableFeatureCollectionInputData_Struct Struct Defines the input data of AddReusableFeatureBuilder

Method Detail

CreateBuilder

AddReusableFeatureCollection.CreateBuilder

Creates a AddReusableFeature builder

Signature CreateBuilder(inputData)

Parameters:inputData (NXOpen.Tooling.AddReusableFeatureCollectionInputData_Struct) – Input data
Returns:Add Reusable Feature Builder
Return type:NXOpen.Tooling.AddReusableFeatureBuilder

New in version NX7.5.0.

License requirements: None.