AddReusableFeatureBuilderLayerOptionType Enumeration

NXOpen.Tooling.AddReusableFeatureBuilder.LayerOptionType is an alias for NXOpen.Tooling.AddReusableFeatureBuilderLayerOptionType

class NXOpen.Tooling.AddReusableFeatureBuilderLayerOptionType

Bases: object

Represents the layer option type

Enum Members

Enum Member Enum Member Description
Work
Work Layer
Original
Original Layer
AsSpecified
As Specified Layer
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.