IsvControlPanelBuilder Class¶
-
class
NXOpen.SIM.
IsvControlPanelBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.SIM.IsvControlPanelBuilder
To create a new instance of this class, use
NXOpen.SIM.KinematicConfigurator.CreateIsvControlPanelBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
IsInHistoryBuffer | Returns the simulation is inside history buffer |
MachineConfiguratorFilename | Returns the machine configurator filename with full path |
SimDebugBuilder | Returns the sim debug builder |
SimulationOptionsBuilder | Returns the simulation options builder |
Tag | Returns the Tag for this object. |
VncStatus | Returns the mode of VNC |
Methods¶
Method | Description |
---|---|
AddIsInHistoryBuffer | Registers the IsInHistoryBufferChanged callback. |
AddSimStop | Registers the SimStop callback. |
AddVncStatus | Registers the VNC Status callback. |
ApplySimulationOptions | Apply the simulation options |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDetailCount | Return the number of Details of the specified type @return |
GetObject | Returns the object currently being edited by this builder. |
GetPostprocessorFilename | Get the post processor definition and tcl filename with full path @return The tcl filename with full path |
GetShow3dMaterialRemoval | Gets the show 3d material removal @return |
GetShowToolPath | Gets the show tool path @return |
GetSingleStep | Gets the single step in Tool Path Based Simulation @return |
GetSingleStepMode | Gets the single step mode in Machine Code Simulation @return |
GetVisualization | Gets the visualization @return |
JumpToDetailsLine | Jump to details line |
JumpToMachineTime | Jump to machine time |
JumpToNcProgramLine | Jump to nc program line in the active channel |
MachineControlClearAlarm | Machine Control Panel: Clear Alarms for all channels |
MachineControlDryRun | Machine Control Panel: Activate Machine Dry Run |
MachineControlFeedRateOverride | Machine Control Panel: Sets Machine Feed Rate Override |
MachineControlGetChannels | Gets the Channel Names @return the names of available channel |
MachineControlGetCycleTime | Gets the Machine Cycle Time @return The cycle time in ms |
MachineControlGetFeedRateOverrideMaximumValue | Machine Control Panel: Gets the Machine Feed Rate Override Maximum Value @return The feed rate override max value |
MachineControlReadVariable | Read Variable e. |
MachineControlResetMachine | Machine Control Panel: Fast Reset Machine |
MachineControlResetNc | Machine Control Panel: NC Reset for all channels |
MachineControlResetPart | Machine Control Panel: Reset Part |
MachineControlSaveMachineData | Machine Control Panel: Save the Machine Data (SRAM) |
MachineControlShowHmi | Machine Control Panel: Show HMI |
MachineControlSingleBlockMode | Machine Control Panel: Activate Machine Single Block Mode |
MachineControlStartNc | Machine Control Panel: NC Start for all channels |
MachineControlStopNc | Machine Control Panel: NC Stop for all channels |
MachineControlWriteVariable | Write Variable e. |
PlayBackward | Simulation Control Panel: Play Backward |
PlayForward | Simulation Control Panel: Play Forward |
PlayToMachineTime | Play to Machine Time |
ReadSettingsFromFile | Read simulation settings from xml file |
RemoveIsInHistoryBuffer | Unregisters the IsInHistoryBufferChanged callback. |
RemoveSimStop | Unregisters the SimStop callback. |
RemoveVncStatus | Unregisters the VNC Status callback. |
ResetMachine | Simulation Control Panel: (Full) Reset Machine |
SaveSettingsToFile | Save simulation settings to xml file |
SetShow3dMaterialRemoval | Sets the show 3d material removal @return The dialog response, if the user don’t define workpiece the autoblock dialog will displayed. |
SetShowToolPath | Sets the show tool path |
SetSingleStep | Sets the single step in Tool Path Based Simulation |
SetSingleStepMode | Sets the single step mode in Machine Code Simulation |
SetSpeed | Simulation Control Panel: Simulation Speed |
SetVisualization | Sets the visualization |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
SingleStepBackward | Simulation Control Panel: Single Step Backward |
SingleStepForward | Simulation Control Panel: Single Step Forward |
StepToNextOperation | Simulation Control Panel: Step to Next Operation |
StepToPreviousOperation | Simulation Control Panel: Step to Previous Operation |
Stop | Simulation Control Panel: Stop the simulation |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
IsvControlPanelBuilderDetailType Enumeration | Type of record reported in the Simulation Details group |
IsvControlPanelBuilderSingleStepModeType Enumeration | The Single Step Mode type that used in :py:class:` NXOpen.SIM.IsvControlPanelBuilderVisualizationType.MachineCodeSimulateCse < NXOpen.SIM.IsvControlPanelBuilderVisualizationType>` simulation mode. |
IsvControlPanelBuilderSingleStepType Enumeration | The Single Step type that used in :py:class:` NXOpen.SIM.IsvControlPanelBuilderVisualizationType.MachineCodeSimulateMtd < NXOpen.SIM.IsvControlPanelBuilderVisualizationType>` or :py:class:` NXOpen.SIM.IsvControlPanelBuilderVisualizationType.ToolPathSimulation < NXOpen.SIM.IsvControlPanelBuilderVisualizationType>` simulation mode. |
IsvControlPanelBuilderVisualizationType Enumeration | The Visualization type |
IsvControlPanelBuilderVncMode Enumeration | Type of VNC Mode |
Property Detail¶
IsInHistoryBuffer¶
-
IsvControlPanelBuilder.
IsInHistoryBuffer
¶ Returns the simulation is inside history buffer
-------------------------------------
Getter Method
Signature
IsInHistoryBuffer()
Returns: Return type: bool New in version NX10.0.3.
License requirements: None.
MachineConfiguratorFilename¶
-
IsvControlPanelBuilder.
MachineConfiguratorFilename
¶ Returns the machine configurator filename with full path
-------------------------------------
Getter Method
Signature
MachineConfiguratorFilename()
Returns: The machine configurator filename with full path Return type: str New in version NX10.0.1.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
SimDebugBuilder¶
-
IsvControlPanelBuilder.
SimDebugBuilder
¶ Returns the sim debug builder
-------------------------------------
Getter Method
Signature
SimDebugBuilder()
Returns: the sim debug builder Return type: NXOpen.SIM.SimDebugBuilder
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
SimulationOptionsBuilder¶
-
IsvControlPanelBuilder.
SimulationOptionsBuilder
¶ Returns the simulation options builder
-------------------------------------
Getter Method
Signature
SimulationOptionsBuilder()
Returns: the simulation options builder Return type: NXOpen.CAM.SimulationOptionsBuilder
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
VncStatus¶
-
IsvControlPanelBuilder.
VncStatus
¶ Returns the mode of VNC
-------------------------------------
Getter Method
Signature
VncStatus()
Returns: Return type: NXOpen.SIM.IsvControlPanelBuilderVncMode
New in version NX10.0.3.
License requirements: None.
Method Detail¶
AddIsInHistoryBuffer¶
-
IsvControlPanelBuilder.
AddIsInHistoryBuffer
¶ Registers the IsInHistoryBufferChanged callback.
Signature
AddIsInHistoryBuffer(handler)
Parameters: handler (CallableObject) – Returns: Return type: int New in version NX10.0.3.
License requirements: None.
AddSimStop¶
-
IsvControlPanelBuilder.
AddSimStop
¶ Registers the SimStop callback.
Signature
AddSimStop(handler)
Parameters: handler (CallableObject) – Returns: Return type: int New in version NX10.0.3.
License requirements: None.
AddVncStatus¶
-
IsvControlPanelBuilder.
AddVncStatus
¶ Registers the VNC Status callback.
Signature
AddVncStatus(handler)
Parameters: handler (CallableObject) – Returns: Return type: int New in version NX10.0.3.
License requirements: None.
ApplySimulationOptions¶
-
IsvControlPanelBuilder.
ApplySimulationOptions
¶ Apply the simulation options
Signature
ApplySimulationOptions()
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
GetDetailCount¶
-
IsvControlPanelBuilder.
GetDetailCount
¶ Return the number of Details of the specified type
Signature
GetDetailCount(type)
Parameters: type ( NXOpen.SIM.IsvControlPanelBuilderDetailType
) –Returns: Return type: int New in version NX10.0.1.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
GetPostprocessorFilename¶
-
IsvControlPanelBuilder.
GetPostprocessorFilename
¶ Get the post processor definition and tcl filename with full path
Signature
GetPostprocessorFilename()
Returns: a tuple Return type: A tuple consisting of (tclFilename, definitionFilename). tclFilename is a str. The tcl filename with full pathdefinitionFilename is a str. The definition filename with full path New in version NX10.0.1.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
GetShow3dMaterialRemoval¶
-
IsvControlPanelBuilder.
GetShow3dMaterialRemoval
¶ Gets the show 3d material removal
Signature
GetShow3dMaterialRemoval()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
GetShowToolPath¶
-
IsvControlPanelBuilder.
GetShowToolPath
¶ Gets the show tool path
Signature
GetShowToolPath()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
GetSingleStep¶
-
IsvControlPanelBuilder.
GetSingleStep
¶ Gets the single step in Tool Path Based Simulation
Signature
GetSingleStep()
Returns: Return type: NXOpen.SIM.IsvControlPanelBuilderSingleStepType
New in version NX8.0.0.
License requirements: None.
GetSingleStepMode¶
-
IsvControlPanelBuilder.
GetSingleStepMode
¶ Gets the single step mode in Machine Code Simulation
Signature
GetSingleStepMode()
Returns: Return type: NXOpen.SIM.IsvControlPanelBuilderSingleStepModeType
New in version NX10.0.2.
License requirements: None.
GetVisualization¶
-
IsvControlPanelBuilder.
GetVisualization
¶ Gets the visualization
Signature
GetVisualization()
Returns: Return type: NXOpen.SIM.IsvControlPanelBuilderVisualizationType
New in version NX8.0.0.
License requirements: None.
JumpToDetailsLine¶
-
IsvControlPanelBuilder.
JumpToDetailsLine
¶ Jump to details line
Signature
JumpToDetailsLine(line)
Parameters: line (int) – The details window line New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
JumpToMachineTime¶
-
IsvControlPanelBuilder.
JumpToMachineTime
¶ Jump to machine time
Signature
JumpToMachineTime(machineTime)
Parameters: machineTime (str) – The machine time in hh:mm:ss.s format New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
JumpToNcProgramLine¶
-
IsvControlPanelBuilder.
JumpToNcProgramLine
¶ Overloaded method JumpToNcProgramLine
JumpToNcProgramLine(line)
JumpToNcProgramLine(channelName, line)
-------------------------------------
Jump to nc program line in the active channel
Signature
JumpToNcProgramLine(line)
Parameters: line (int) – The nc program window line New in version NX8.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
-------------------------------------
Jump to nc program line in the specified channel
Signature
JumpToNcProgramLine(channelName, line)
Parameters: - channelName (str) – The channel name. If this is None or empty the active channel will be used.
- line (int) – The nc program line
New in version NX11.0.1.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
-------------------------------------
MachineControlClearAlarm¶
-
IsvControlPanelBuilder.
MachineControlClearAlarm
¶ Overloaded method MachineControlClearAlarm
MachineControlClearAlarm()
MachineControlClearAlarm(channels)
-------------------------------------
Machine Control Panel: Clear Alarms for all channels
Signature
MachineControlClearAlarm()
New in version NX8.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
-------------------------------------
Machine Control Panel: Clear Alarms for specific channels
Signature
MachineControlClearAlarm(channels)
Parameters: channels (list of str) – New in version NX9.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
-------------------------------------
MachineControlDryRun¶
-
IsvControlPanelBuilder.
MachineControlDryRun
¶ Machine Control Panel: Activate Machine Dry Run
Signature
MachineControlDryRun(enable)
Parameters: enable (bool) – Enable or disable the dry run New in version NX8.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
MachineControlFeedRateOverride¶
-
IsvControlPanelBuilder.
MachineControlFeedRateOverride
¶ Machine Control Panel: Sets Machine Feed Rate Override
Signature
MachineControlFeedRateOverride(value)
Parameters: value (int) – The feed rate override value New in version NX8.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
MachineControlGetChannels¶
-
IsvControlPanelBuilder.
MachineControlGetChannels
¶ Gets the Channel Names
Signature
MachineControlGetChannels()
Returns: the names of available channel Return type: list of str New in version NX9.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
MachineControlGetCycleTime¶
-
IsvControlPanelBuilder.
MachineControlGetCycleTime
¶ Gets the Machine Cycle Time
Signature
MachineControlGetCycleTime()
Returns: The cycle time in ms Return type: int New in version NX9.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
MachineControlGetFeedRateOverrideMaximumValue¶
-
IsvControlPanelBuilder.
MachineControlGetFeedRateOverrideMaximumValue
¶ Machine Control Panel: Gets the Machine Feed Rate Override Maximum Value
Signature
MachineControlGetFeedRateOverrideMaximumValue()
Returns: The feed rate override max value Return type: int New in version NX9.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
MachineControlReadVariable¶
-
IsvControlPanelBuilder.
MachineControlReadVariable
¶ Read Variable e.
- VDI Variable, Machine Data
Signature
MachineControlReadVariable(channelName, variableName)
Parameters: - channelName (str) – The channel name, NULL or empty means all channels
- variableName (str) – The variable name
Returns: a tuple
Return type: A tuple consisting of (success, variableValue, variableType). success is a bool. variableValue is a str. The variable valuevariableType is a str. The variable type: VDI_SWITCH, VDI_INTEGER, VDI_SINGLESTEP
New in version NX9.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
MachineControlResetMachine¶
-
IsvControlPanelBuilder.
MachineControlResetMachine
¶ Machine Control Panel: Fast Reset Machine
Signature
MachineControlResetMachine()
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
MachineControlResetNc¶
-
IsvControlPanelBuilder.
MachineControlResetNc
¶ Overloaded method MachineControlResetNc
MachineControlResetNc()
MachineControlResetNc(channels)
-------------------------------------
Machine Control Panel: NC Reset for all channels
Signature
MachineControlResetNc()
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
-------------------------------------
Machine Control Panel: NC Reset for specific channels
Signature
MachineControlResetNc(channels)
Parameters: channels (list of str) – New in version NX9.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
-------------------------------------
MachineControlResetPart¶
-
IsvControlPanelBuilder.
MachineControlResetPart
¶ Machine Control Panel: Reset Part
Signature
MachineControlResetPart()
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
MachineControlSaveMachineData¶
-
IsvControlPanelBuilder.
MachineControlSaveMachineData
¶ Machine Control Panel: Save the Machine Data (SRAM)
Signature
MachineControlSaveMachineData()
New in version NX8.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
MachineControlShowHmi¶
-
IsvControlPanelBuilder.
MachineControlShowHmi
¶ Machine Control Panel: Show HMI
Signature
MachineControlShowHmi()
New in version NX8.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
MachineControlSingleBlockMode¶
-
IsvControlPanelBuilder.
MachineControlSingleBlockMode
¶ Machine Control Panel: Activate Machine Single Block Mode
Signature
MachineControlSingleBlockMode(enable)
Parameters: enable (bool) – Enable or disable the single block mode New in version NX8.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
MachineControlStartNc¶
-
IsvControlPanelBuilder.
MachineControlStartNc
¶ Overloaded method MachineControlStartNc
MachineControlStartNc()
MachineControlStartNc(channels)
-------------------------------------
Machine Control Panel: NC Start for all channels
Signature
MachineControlStartNc()
New in version NX9.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
-------------------------------------
Machine Control Panel: NC Start for specific channels
Signature
MachineControlStartNc(channels)
Parameters: channels (list of str) – New in version NX9.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
-------------------------------------
MachineControlStopNc¶
-
IsvControlPanelBuilder.
MachineControlStopNc
¶ Overloaded method MachineControlStopNc
MachineControlStopNc()
MachineControlStopNc(channels)
-------------------------------------
Machine Control Panel: NC Stop for all channels
Signature
MachineControlStopNc()
New in version NX9.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
-------------------------------------
Machine Control Panel: NC Stop for specific channels
Signature
MachineControlStopNc(channels)
Parameters: channels (list of str) – New in version NX9.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
-------------------------------------
MachineControlWriteVariable¶
-
IsvControlPanelBuilder.
MachineControlWriteVariable
¶ Write Variable e.
- VDI Variable, Machine Data
Signature
MachineControlWriteVariable(channelName, variableName, variableValue, variableType)
Parameters: - channelName (str) – The channel name, NULL or empty means all channels
- variableName (str) – The variable name
- variableValue (str) – The variable value
- variableType (str) – The variable type: VDI_SWITCH, VDI_INTEGER, VDI_SINGLESTEP
Returns: Return type: bool
New in version NX9.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
PlayBackward¶
-
IsvControlPanelBuilder.
PlayBackward
¶ Simulation Control Panel: Play Backward
Signature
PlayBackward()
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
PlayForward¶
-
IsvControlPanelBuilder.
PlayForward
¶ Simulation Control Panel: Play Forward
Signature
PlayForward()
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
PlayToMachineTime¶
-
IsvControlPanelBuilder.
PlayToMachineTime
¶ Play to Machine Time
Signature
PlayToMachineTime(machineTime)
Parameters: machineTime (str) – The machine time in hh:mm:ss.s format New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
ReadSettingsFromFile¶
-
IsvControlPanelBuilder.
ReadSettingsFromFile
¶ Read simulation settings from xml file
Signature
ReadSettingsFromFile(filename)
Parameters: filename (str) – New in version NX9.0.1.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
RemoveIsInHistoryBuffer¶
-
IsvControlPanelBuilder.
RemoveIsInHistoryBuffer
¶ Unregisters the IsInHistoryBufferChanged callback.
Signature
RemoveIsInHistoryBuffer(handlerId)
Parameters: handlerId (int) – Returns: Return type: bool New in version NX10.0.3.
License requirements: None.
RemoveSimStop¶
-
IsvControlPanelBuilder.
RemoveSimStop
¶ Unregisters the SimStop callback.
Signature
RemoveSimStop(handlerId)
Parameters: handlerId (int) – Returns: Return type: bool New in version NX10.0.3.
License requirements: None.
RemoveVncStatus¶
-
IsvControlPanelBuilder.
RemoveVncStatus
¶ Unregisters the VNC Status callback.
Signature
RemoveVncStatus(handlerId)
Parameters: handlerId (int) – Returns: Return type: bool New in version NX10.0.3.
License requirements: None.
ResetMachine¶
-
IsvControlPanelBuilder.
ResetMachine
¶ Simulation Control Panel: (Full) Reset Machine
Signature
ResetMachine()
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
SaveSettingsToFile¶
-
IsvControlPanelBuilder.
SaveSettingsToFile
¶ Save simulation settings to xml file
Signature
SaveSettingsToFile(filename)
Parameters: filename (str) – New in version NX9.0.1.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
SetShow3dMaterialRemoval¶
-
IsvControlPanelBuilder.
SetShow3dMaterialRemoval
¶ Sets the show 3d material removal
Signature
SetShow3dMaterialRemoval(state)
Parameters: state (bool) – The state Returns: The dialog response, if the user don’t define workpiece the autoblock dialog will displayed. And if the user cancel it the response is UGII_CANCEL :rtype: int
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
SetShowToolPath¶
-
IsvControlPanelBuilder.
SetShowToolPath
¶ Sets the show tool path
Signature
SetShowToolPath(state)
Parameters: state (bool) – The state New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
SetSingleStep¶
-
IsvControlPanelBuilder.
SetSingleStep
¶ Sets the single step in Tool Path Based Simulation
Signature
SetSingleStep(type)
Parameters: type ( NXOpen.SIM.IsvControlPanelBuilderSingleStepType
) – The single step typeNew in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
SetSingleStepMode¶
-
IsvControlPanelBuilder.
SetSingleStepMode
¶ Sets the single step mode in Machine Code Simulation
Signature
SetSingleStepMode(type)
Parameters: type ( NXOpen.SIM.IsvControlPanelBuilderSingleStepModeType
) – The single step mode typeNew in version NX10.0.2.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
SetSpeed¶
-
IsvControlPanelBuilder.
SetSpeed
¶ Simulation Control Panel: Simulation Speed
Signature
SetSpeed(simSpeed)
Parameters: simSpeed (int) – The simulation speed New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
SetVisualization¶
-
IsvControlPanelBuilder.
SetVisualization
¶ Sets the visualization
Signature
SetVisualization(type)
Parameters: type ( NXOpen.SIM.IsvControlPanelBuilderVisualizationType
) – The visualization typeNew in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
SingleStepBackward¶
-
IsvControlPanelBuilder.
SingleStepBackward
¶ Simulation Control Panel: Single Step Backward
Signature
SingleStepBackward()
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
SingleStepForward¶
-
IsvControlPanelBuilder.
SingleStepForward
¶ Simulation Control Panel: Single Step Forward
Signature
SingleStepForward()
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
StepToNextOperation¶
-
IsvControlPanelBuilder.
StepToNextOperation
¶ Simulation Control Panel: Step to Next Operation
Signature
StepToNextOperation()
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
StepToPreviousOperation¶
-
IsvControlPanelBuilder.
StepToPreviousOperation
¶ Simulation Control Panel: Step to Previous Operation
Signature
StepToPreviousOperation()
New in version NX8.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
Stop¶
-
IsvControlPanelBuilder.
Stop
¶ Simulation Control Panel: Stop the simulation
Signature
Stop()
New in version NX9.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”)
Validate¶
-
IsvControlPanelBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.