IsvControlPanelBuilderVncMode Enumeration¶
NXOpen.SIM.IsvControlPanelBuilder.VncMode is an alias for NXOpen.SIM.IsvControlPanelBuilderVncMode
-
class
NXOpen.SIM.
IsvControlPanelBuilderVncMode
¶ Bases:
object
Type of VNC Mode
Enum Members
Enum Member Enum Member Description Error ERRORNotconnected NOT CONNECTEDConnected CONNECTEDBooted BOOTEDConfigured CONFIGUREDInitialized INITIALIZEDProgramsLoaded PROGRAMS LOADEDReset RESETStop STOPStart STARTRun RUN-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-