SessionVisualizationPerformance Class¶
-
class
NXOpen.Preferences.
SessionVisualizationPerformance
¶ Bases:
object
Represents visualization performance preferences that are applicable to the entire session.
To obtain an instance of this class, refer to
NXOpen.Preferences.SessionPreferences
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
RenderSolidsUsingStoredFacets | Returns or sets the rendering of solids using stored facets during interactive mode. |
Methods¶
Property Detail¶
RenderSolidsUsingStoredFacets¶
-
SessionVisualizationPerformance.
RenderSolidsUsingStoredFacets
¶ Returns or sets the rendering of solids using stored facets during interactive mode.
When a solid is rendered in non-lightweight mode, this preference can be enabled to use facets stored in the part if valid facets exist for the solid, even if those facets do not meet the current rendering parameters. This improves performance of certain shaded displays by avoiding need to tessellate the solid, though the visual quality may be impacted. E.g. when this preference is enabled, smooth edge settings (e.g. see use of
NXOpen.Preferences.ViewVisualizationVisualSmoothEdgeWidth
) are implicitly ignored to improve the performance.This setting is ignored by
NXOpen.ViewCollection.UpdateDisplay()
.The display is not immediately regenerated when this setting is changed. Use
NXOpen.ViewCollection.Regenerate()
to update display.-------------------------------------
Getter Method
Signature
RenderSolidsUsingStoredFacets()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RenderSolidsUsingStoredFacets(useStoredFacets)
Parameters: useStoredFacets (bool) – New in version NX11.0.0.
License requirements: None.