PartSheetmetal Class¶
-
class
NXOpen.Preferences.
PartSheetmetal
¶ Bases:
object
Represents the NX Sheetmetal preferences applicable to part
Preferences are in control of the part. They can not be created but can only be changed.
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits and applies all the settings done with set_callout_type_display and set_object_type_display. |
GetBendAllowanceFormula | RETURNS the bend allowance formula @return bend allowance formula |
GetBendDefinitionMethodOption | RETURNS the bend definition method @return bend definition method option |
GetBendRadius | RETURNS the bend radius expression @return expression object for radius of bend faces |
GetBendReliefDepth | RETURNS the bend relief depth @return expression object for depth of bend relief |
GetBendReliefWidth | RETURNS the bend relief width @return expression object for width of bend relief |
GetBendTable | RETURNS the bend table name @return bend table name |
GetDepthThreshold | RETURNS the depth threshold @return expression object for depth threshold of joggle |
GetDeviationalToleranceInFlatSolid | RETURNS the deviational tolerance during Flat Solid simplification @return flag |
GetDistanceThreshold | RETURNS the distance threshold @return expression object for distance threshold of joggle |
GetFlatPatternAllCalloutTypeDisplay | Returns the dialog names, identifiers, and enabled status for all the available callout types. |
GetFlatPatternAllObjectTypeDisplay | Returns the types, colors, fonts, widths, and enabled status for all the the available object types. |
GetFlatPatternCalloutOrientationType | Returns the orientation type for flat pattern callouts. |
GetFlatPatternCalloutTypeContents | Returns the contents for a callout type. |
GetFlatPatternCalloutTypeDisplay | Returns the display data for a callout type. |
GetFlatPatternObjectTypeDisplay | Returns the display data for a flat pattern object type. |
GetFlexibleCableBottomFaceColor | RETURNS the bottom face color. |
GetFlexibleCableTopFaceColor | RETURNS the top face color. |
GetInnerCornerTreatmentType | RETURNS the inner corner treatment type in Flat as Solid operation @return outer corner treatment type |
GetInnerCornerTreatmentValue | RETURNS the inner corner treatment value for Flat as Solid operations @return expression object for inner corner treatment value |
GetIsBsplineSimplifiedInFlatSolid | RETURNS the flag indicating whether B-Splines are simplified as part of the Flat Solid creation @return flag |
GetIsSystemGeneratedBendReliefRemovedInFlatSolid | RETURNS the flag indicating whether or not system generated bend releifs are removed as part of the Flat Solid creation @return flag |
GetMaintainCircularShapeForHolesInFlatSolid | Returns the flag indicating whether or not maintain circular shape for holes as part of the Flat Solid creation @return flag |
GetMaterial | RETURNS the material name saved with the part @return The name of the material saved with the part |
GetMaterialNames | RETURNS the material names defined in the material standards table @return |
GetMaterialProperties | RETURNS the material name saved with the part @return property Values |
GetMinimumArcToleranceInFlatSolid | RETURNS the minimum arc tolerance during Flat Solid simplification @return flag |
GetMinimumToolClearance | Returns the minimum tool clearance expression @return expression object for punch tool clearance |
GetMinimumWebLength | Returns the minimum Web Length expression @return expression object for Web Length |
GetNeutralFactor | RETURNS the neutral factor @return expression object for neutral factor of bend areas |
GetOffsetRadius | RETURNS the offset radius @return expression object for offset radius of joggle |
GetOuterCornerTreatmentType | RETURNS the outer corner treatment type in Flat as Solid operation @return outer corner treatment type |
GetOuterCornerTreatmentValue | RETURNS the out corner treatment value for Flat as Solid operations @return expression object for out corner treatment value |
GetStationaryRadius | RETURNS the stationary radius @return expression object for stationary radius of joggle |
GetThickness | RETURNS the thickness expression @return expression object for sheet thickness |
GetTool | Returns the tool name saved with the part @return The name of the tool saved with the part |
GetToolNames | Returns the tool names defined in the material standards table @return |
GetToolProperties | Returns the tool properties saved with the part @return property Values |
SetBendAllowanceFormula | SETS the bend allowance formula |
SetBendDefinitionMethodOption | SETS the bend definition method |
SetBendRadius | The bend radius value |
SetBendReliefDepth | THE bend relief depth value |
SetBendReliefWidth | THE bend relief depth value |
SetBendTable | SETS the bend table name |
SetDepthThreshold | THE depth threshold |
SetDeviationalToleranceInFlatSolid | SETS the deviational tolerance during Flat Solid simplification |
SetDistanceThreshold | THE distance threshold |
SetFlatPatternCalloutOrientationType | Sets the orientation type for flat pattern callouts. |
SetFlatPatternCalloutTypeContents | Sets the contents for a callout type. |
SetFlatPatternCalloutTypeDisplay | Sets the display data for a callout type. |
SetFlatPatternObjectTypeDisplay | Sets the display data for a flat pattern object type. |
SetFlexibleCableBottomFaceColor | THE bottom face color. |
SetFlexibleCableTopFaceColor | THE top face color. |
SetInnerCornerTreatmentType | SETS the inner corner treatment type in Flat as Solid operation |
SetInnerCornerTreatmentValue | SETS the inner corner treatment value for Flat as Solid operations |
SetIsBsplineSimplifiedInFlatSolid | SETS the flag indicating whether or not B-Splines are simplified as part of the Flat Solid creation |
SetIsSystemGeneratedBendReliefRemovedInFlatSolid | SETS the flag indicating whether or not system generated bend releifs are removed as part of the Flat Solid creation |
SetMaintainCircularShapeForHolesInFlatSolid | Sets the flag indicating whether or not maintain circular shape for holes as part of the Flat Solid creation |
SetMaterial | The material standard |
SetMinimumArcToleranceInFlatSolid | SETS the minimum arc tolerance during Flat Solid simplification |
SetMinimumToolClearance | Sets minimum tool clearance expression |
SetMinimumWebLength | Sets minimum Web Length expression |
SetNeutralFactor | THE bend relief depth value |
SetOffsetRadius | THE offset radius |
SetOuterCornerTreatmentType | SETS the outer corner treatment type in Flat as Solid operation |
SetOuterCornerTreatmentValue | THE outer corner treatment value for Flat as Solid operations |
SetStationaryRadius | THE stationary radius |
SetThickness | THE thickness value string |
SetTool | The tool standard |
Enumerations¶
PartSheetmetalBendDefinitionMethodOptions Enumeration | This enum represents the bend definition method options in preferences. |
PartSheetmetalFlatPatternCalloutOrientationType Enumeration | This enum represents orientation types for the flat pattern callouts |
PartSheetmetalFlatPatternObjectType Enumeration | The members of the following enumerated type are used to identify object types to the FlatPattern API. |
Structs¶
PartSheetmetalFlatPatternCalloutTypeDisplay_Struct Struct | The members of the following structure are the display data for a callout in a flat pattern drawing member view. |
PartSheetmetalFlatPatternObjectTypeDisplay_Struct Struct | The members of the following structure are the display data for an object in a flat pattern drawing member view. |
Method Detail¶
Commit¶
-
PartSheetmetal.
Commit
¶ Commits and applies all the settings done with set_callout_type_display and set_object_type_display.
It must be called after a sequence of calls to those methods to cause the view to update.
Signature
Commit()
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetBendAllowanceFormula¶
-
PartSheetmetal.
GetBendAllowanceFormula
¶ RETURNS the bend allowance formula
Signature
GetBendAllowanceFormula()
Returns: bend allowance formula Return type: str New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetBendDefinitionMethodOption¶
-
PartSheetmetal.
GetBendDefinitionMethodOption
¶ RETURNS the bend definition method
Signature
GetBendDefinitionMethodOption()
Returns: bend definition method option Return type: NXOpen.Preferences.PartSheetmetalBendDefinitionMethodOptions
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetBendRadius¶
-
PartSheetmetal.
GetBendRadius
¶ RETURNS the bend radius expression
Signature
GetBendRadius()
Returns: expression object for radius of bend faces Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetBendReliefDepth¶
-
PartSheetmetal.
GetBendReliefDepth
¶ RETURNS the bend relief depth
Signature
GetBendReliefDepth()
Returns: expression object for depth of bend relief Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetBendReliefWidth¶
-
PartSheetmetal.
GetBendReliefWidth
¶ RETURNS the bend relief width
Signature
GetBendReliefWidth()
Returns: expression object for width of bend relief Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetBendTable¶
-
PartSheetmetal.
GetBendTable
¶ RETURNS the bend table name
Signature
GetBendTable()
Returns: bend table name Return type: str New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetDepthThreshold¶
-
PartSheetmetal.
GetDepthThreshold
¶ RETURNS the depth threshold
Signature
GetDepthThreshold()
Returns: expression object for depth threshold of joggle Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
GetDeviationalToleranceInFlatSolid¶
-
PartSheetmetal.
GetDeviationalToleranceInFlatSolid
¶ RETURNS the deviational tolerance during Flat Solid simplification
Signature
GetDeviationalToleranceInFlatSolid()
Returns: flag Return type: float New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetDistanceThreshold¶
-
PartSheetmetal.
GetDistanceThreshold
¶ RETURNS the distance threshold
Signature
GetDistanceThreshold()
Returns: expression object for distance threshold of joggle Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
GetFlatPatternAllCalloutTypeDisplay¶
-
PartSheetmetal.
GetFlatPatternAllCalloutTypeDisplay
¶ Returns the dialog names, identifiers, and enabled status for all the available callout types.
Signature
GetFlatPatternAllCalloutTypeDisplay()
Returns: Array of structures with the callout type display data. Return type: list of NXOpen.Preferences.PartSheetmetalFlatPatternCalloutTypeDisplay_Struct
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetFlatPatternAllObjectTypeDisplay¶
-
PartSheetmetal.
GetFlatPatternAllObjectTypeDisplay
¶ Returns the types, colors, fonts, widths, and enabled status for all the the available object types.
Signature
GetFlatPatternAllObjectTypeDisplay()
Returns: Array of structures with the object type display data. Return type: list of NXOpen.Preferences.PartSheetmetalFlatPatternObjectTypeDisplay_Struct
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetFlatPatternCalloutOrientationType¶
-
PartSheetmetal.
GetFlatPatternCalloutOrientationType
¶ Returns the orientation type for flat pattern callouts.
Signature
GetFlatPatternCalloutOrientationType()
Returns: The orientation type for the flat pattern callouts. Return type: NXOpen.Preferences.PartSheetmetalFlatPatternCalloutOrientationType
New in version NX9.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetFlatPatternCalloutTypeContents¶
-
PartSheetmetal.
GetFlatPatternCalloutTypeContents
¶ Returns the contents for a callout type.
Signature
GetFlatPatternCalloutTypeContents(calloutType)
Parameters: calloutType (str) – The name of the callout type for which to get the content. Returns: The contents for the callout type. Return type: list of str New in version NX9.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetFlatPatternCalloutTypeDisplay¶
-
PartSheetmetal.
GetFlatPatternCalloutTypeDisplay
¶ Returns the display data for a callout type.
The name member of the
NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlatPatternCalloutTypeDisplay_Struct
is separately allocated from the callout_type argument string. In some cases the new string will contain an extended form of the callout_type passed in, and that form should be used for subsequent JA calls, without modification.Signature
GetFlatPatternCalloutTypeDisplay(calloutType)
Parameters: calloutType (str) – The name of the callout type for which to get the display data. Returns: The display data for the callout type. Return type: NXOpen.Preferences.PartSheetmetalFlatPatternCalloutTypeDisplay_Struct
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetFlatPatternObjectTypeDisplay¶
-
PartSheetmetal.
GetFlatPatternObjectTypeDisplay
¶ Returns the display data for a flat pattern object type.
Signature
GetFlatPatternObjectTypeDisplay(objectType)
Parameters: objectType ( NXOpen.Preferences.PartSheetmetalFlatPatternObjectType
) – The object type for which to return the display data.Returns: The display data for the flat pattern object type. Return type: NXOpen.Preferences.PartSheetmetalFlatPatternObjectTypeDisplay_Struct
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetFlexibleCableBottomFaceColor¶
GetFlexibleCableTopFaceColor¶
GetInnerCornerTreatmentType¶
-
PartSheetmetal.
GetInnerCornerTreatmentType
¶ RETURNS the inner corner treatment type in Flat as Solid operation
Signature
GetInnerCornerTreatmentType()
Returns: outer corner treatment type Return type: NXOpen.Features.SheetMetal.FeatureProperty
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetInnerCornerTreatmentValue¶
-
PartSheetmetal.
GetInnerCornerTreatmentValue
¶ RETURNS the inner corner treatment value for Flat as Solid operations
Signature
GetInnerCornerTreatmentValue()
Returns: expression object for inner corner treatment value Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetIsBsplineSimplifiedInFlatSolid¶
-
PartSheetmetal.
GetIsBsplineSimplifiedInFlatSolid
¶ RETURNS the flag indicating whether B-Splines are simplified as part of the Flat Solid creation
Signature
GetIsBsplineSimplifiedInFlatSolid()
Returns: flag Return type: bool New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetIsSystemGeneratedBendReliefRemovedInFlatSolid¶
-
PartSheetmetal.
GetIsSystemGeneratedBendReliefRemovedInFlatSolid
¶ RETURNS the flag indicating whether or not system generated bend releifs are removed as part of the Flat Solid creation
Signature
GetIsSystemGeneratedBendReliefRemovedInFlatSolid()
Returns: flag Return type: bool New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetMaintainCircularShapeForHolesInFlatSolid¶
-
PartSheetmetal.
GetMaintainCircularShapeForHolesInFlatSolid
¶ Returns the flag indicating whether or not maintain circular shape for holes as part of the Flat Solid creation
Signature
GetMaintainCircularShapeForHolesInFlatSolid()
Returns: flag Return type: bool New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetMaterial¶
-
PartSheetmetal.
GetMaterial
¶ RETURNS the material name saved with the part
Signature
GetMaterial()
Returns: The name of the material saved with the part Return type: str New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetMaterialNames¶
-
PartSheetmetal.
GetMaterialNames
¶ RETURNS the material names defined in the material standards table
Signature
GetMaterialNames()
Returns: Return type: list of str New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetMaterialProperties¶
-
PartSheetmetal.
GetMaterialProperties
¶ RETURNS the material name saved with the part
Signature
GetMaterialProperties(materialName)
Parameters: materialName (str) – material Name Returns: a tuple Return type: A tuple consisting of (propertyValues, propertyNames). propertyValues is a list of str. property Values propertyNames is a list of str. property Names New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetMinimumArcToleranceInFlatSolid¶
-
PartSheetmetal.
GetMinimumArcToleranceInFlatSolid
¶ RETURNS the minimum arc tolerance during Flat Solid simplification
Signature
GetMinimumArcToleranceInFlatSolid()
Returns: flag Return type: float New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetMinimumToolClearance¶
-
PartSheetmetal.
GetMinimumToolClearance
¶ Returns the minimum tool clearance expression
Signature
GetMinimumToolClearance()
Returns: expression object for punch tool clearance Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetMinimumWebLength¶
-
PartSheetmetal.
GetMinimumWebLength
¶ Returns the minimum Web Length expression
Signature
GetMinimumWebLength()
Returns: expression object for Web Length Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetNeutralFactor¶
-
PartSheetmetal.
GetNeutralFactor
¶ RETURNS the neutral factor
Signature
GetNeutralFactor()
Returns: expression object for neutral factor of bend areas Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetOffsetRadius¶
-
PartSheetmetal.
GetOffsetRadius
¶ RETURNS the offset radius
Signature
GetOffsetRadius()
Returns: expression object for offset radius of joggle Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
GetOuterCornerTreatmentType¶
-
PartSheetmetal.
GetOuterCornerTreatmentType
¶ RETURNS the outer corner treatment type in Flat as Solid operation
Signature
GetOuterCornerTreatmentType()
Returns: outer corner treatment type Return type: NXOpen.Features.SheetMetal.FeatureProperty
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetOuterCornerTreatmentValue¶
-
PartSheetmetal.
GetOuterCornerTreatmentValue
¶ RETURNS the out corner treatment value for Flat as Solid operations
Signature
GetOuterCornerTreatmentValue()
Returns: expression object for out corner treatment value Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetStationaryRadius¶
-
PartSheetmetal.
GetStationaryRadius
¶ RETURNS the stationary radius
Signature
GetStationaryRadius()
Returns: expression object for stationary radius of joggle Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
GetThickness¶
-
PartSheetmetal.
GetThickness
¶ RETURNS the thickness expression
Signature
GetThickness()
Returns: expression object for sheet thickness Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetTool¶
-
PartSheetmetal.
GetTool
¶ Returns the tool name saved with the part
Signature
GetTool()
Returns: The name of the tool saved with the part Return type: str New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetToolNames¶
-
PartSheetmetal.
GetToolNames
¶ Returns the tool names defined in the material standards table
Signature
GetToolNames()
Returns: Return type: list of str New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetToolProperties¶
-
PartSheetmetal.
GetToolProperties
¶ Returns the tool properties saved with the part
Signature
GetToolProperties(toolName)
Parameters: toolName (str) – tool Name Returns: a tuple Return type: A tuple consisting of (propertyValues, propertyNames). propertyValues is a list of str. property Values propertyNames is a list of str. property Names New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetBendAllowanceFormula¶
-
PartSheetmetal.
SetBendAllowanceFormula
¶ SETS the bend allowance formula
Signature
SetBendAllowanceFormula(updateModel, bendAllowanceFormula)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- bendAllowanceFormula (str) – bend allowance formula
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetBendDefinitionMethodOption¶
-
PartSheetmetal.
SetBendDefinitionMethodOption
¶ SETS the bend definition method
Signature
SetBendDefinitionMethodOption(updateModel, bendDefinitionMethod)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- bendDefinitionMethod (
NXOpen.Preferences.PartSheetmetalBendDefinitionMethodOptions
) – bend definition method option
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetBendRadius¶
-
PartSheetmetal.
SetBendRadius
¶ The bend radius value
Signature
SetBendRadius(updateModel, bendRadius)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- bendRadius (str) – default bend radius value for bend faces
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetBendReliefDepth¶
-
PartSheetmetal.
SetBendReliefDepth
¶ THE bend relief depth value
Signature
SetBendReliefDepth(updateModel, bendReliefDepth)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- bendReliefDepth (str) – default depth value for bend relief
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetBendReliefWidth¶
-
PartSheetmetal.
SetBendReliefWidth
¶ THE bend relief depth value
Signature
SetBendReliefWidth(updateModel, bendReliefWidth)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- bendReliefWidth (str) – default width value for bend relief
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetBendTable¶
-
PartSheetmetal.
SetBendTable
¶ SETS the bend table name
Signature
SetBendTable(updateModel, bendTable)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- bendTable (str) – bend table name
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetDepthThreshold¶
-
PartSheetmetal.
SetDepthThreshold
¶ THE depth threshold
Signature
SetDepthThreshold(updateModel, depthThreshold)
Parameters: - updateModel (bool) – Specifies whether the solid model be updated immediately
- depthThreshold (str) – default depth threshold for joggle
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
SetDeviationalToleranceInFlatSolid¶
-
PartSheetmetal.
SetDeviationalToleranceInFlatSolid
¶ SETS the deviational tolerance during Flat Solid simplification
Signature
SetDeviationalToleranceInFlatSolid(updateModel, deviationalToleranceInFlatSolid)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- deviationalToleranceInFlatSolid (float) – flag
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetDistanceThreshold¶
-
PartSheetmetal.
SetDistanceThreshold
¶ THE distance threshold
Signature
SetDistanceThreshold(updateModel, distanceThreshold)
Parameters: - updateModel (bool) – Specifies whether the solid model be updated immediately
- distanceThreshold (str) – default distance threshold for joggle
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
SetFlatPatternCalloutOrientationType¶
-
PartSheetmetal.
SetFlatPatternCalloutOrientationType
¶ Sets the orientation type for flat pattern callouts.
Signature
SetFlatPatternCalloutOrientationType(orientation)
Parameters: orientation ( NXOpen.Preferences.PartSheetmetalFlatPatternCalloutOrientationType
) – The orientation type for the flat pattern callouts.New in version NX9.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetFlatPatternCalloutTypeContents¶
-
PartSheetmetal.
SetFlatPatternCalloutTypeContents
¶ Sets the contents for a callout type.
Signature
SetFlatPatternCalloutTypeContents(calloutType, contents)
Parameters: - calloutType (str) – The name of the callout type for which to set the content.
- contents (list of str) – The contents for the callout type.
New in version NX9.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetFlatPatternCalloutTypeDisplay¶
-
PartSheetmetal.
SetFlatPatternCalloutTypeDisplay
¶ Sets the display data for a callout type.
Signature
SetFlatPatternCalloutTypeDisplay(calloutType, displayData)
Parameters: - calloutType (str) – The name of the callout type for which to set the display data.
- displayData (
NXOpen.Preferences.PartSheetmetalFlatPatternCalloutTypeDisplay_Struct
) – The display data for the callout type.
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetFlatPatternObjectTypeDisplay¶
-
PartSheetmetal.
SetFlatPatternObjectTypeDisplay
¶ Sets the display data for a flat pattern object type.
Signature
SetFlatPatternObjectTypeDisplay(updateModel, objectType, displayData)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately.
- objectType (
NXOpen.Preferences.PartSheetmetalFlatPatternObjectType
) – The object type for which to get the display data. - displayData (
NXOpen.Preferences.PartSheetmetalFlatPatternObjectTypeDisplay_Struct
) – The display data for the flat pattern object type.
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetFlexibleCableBottomFaceColor¶
SetFlexibleCableTopFaceColor¶
SetInnerCornerTreatmentType¶
-
PartSheetmetal.
SetInnerCornerTreatmentType
¶ SETS the inner corner treatment type in Flat as Solid operation
Signature
SetInnerCornerTreatmentType(updateModel, innerCornerTreatmentType)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- innerCornerTreatmentType (
NXOpen.Features.SheetMetal.FeatureProperty
) – outer corner treatment type
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetInnerCornerTreatmentValue¶
-
PartSheetmetal.
SetInnerCornerTreatmentValue
¶ SETS the inner corner treatment value for Flat as Solid operations
Signature
SetInnerCornerTreatmentValue(updateModel, innerCornerTreatment)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- innerCornerTreatment (str) – default value for inner corner treatment
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetIsBsplineSimplifiedInFlatSolid¶
-
PartSheetmetal.
SetIsBsplineSimplifiedInFlatSolid
¶ SETS the flag indicating whether or not B-Splines are simplified as part of the Flat Solid creation
Signature
SetIsBsplineSimplifiedInFlatSolid(updateModel, isBsplineSimplifiedInFlatSolid)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- isBsplineSimplifiedInFlatSolid (bool) – flag
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetIsSystemGeneratedBendReliefRemovedInFlatSolid¶
-
PartSheetmetal.
SetIsSystemGeneratedBendReliefRemovedInFlatSolid
¶ SETS the flag indicating whether or not system generated bend releifs are removed as part of the Flat Solid creation
Signature
SetIsSystemGeneratedBendReliefRemovedInFlatSolid(updateModel, isSystemGeneratedBendReliefRemoved)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- isSystemGeneratedBendReliefRemoved (bool) – flag
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetMaintainCircularShapeForHolesInFlatSolid¶
-
PartSheetmetal.
SetMaintainCircularShapeForHolesInFlatSolid
¶ Sets the flag indicating whether or not maintain circular shape for holes as part of the Flat Solid creation
Signature
SetMaintainCircularShapeForHolesInFlatSolid(updateModel, isMaintainCircularShapeForHoles)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- isMaintainCircularShapeForHoles (bool) – flag
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetMaterial¶
-
PartSheetmetal.
SetMaterial
¶ The material standard
Signature
SetMaterial(updateModel, standardName)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- standardName (str) – The name of a material from the material standards file
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetMinimumArcToleranceInFlatSolid¶
-
PartSheetmetal.
SetMinimumArcToleranceInFlatSolid
¶ SETS the minimum arc tolerance during Flat Solid simplification
Signature
SetMinimumArcToleranceInFlatSolid(updateModel, minimumArcToleranceInFlatSolid)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- minimumArcToleranceInFlatSolid (float) – flag
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetMinimumToolClearance¶
-
PartSheetmetal.
SetMinimumToolClearance
¶ Sets minimum tool clearance expression
Signature
SetMinimumToolClearance(updateModel, minToolClearance)
Parameters: - updateModel (bool) – Specifies whether the model be updated immediately
- minToolClearance (str) – minimum tool clearance value for NX Sheetmetal model
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetMinimumWebLength¶
-
PartSheetmetal.
SetMinimumWebLength
¶ Sets minimum Web Length expression
Signature
SetMinimumWebLength(updateModel, minWebLength)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- minWebLength (str) – minimum Web Length value for NX Sheetmetal model
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetNeutralFactor¶
-
PartSheetmetal.
SetNeutralFactor
¶ THE bend relief depth value
Signature
SetNeutralFactor(updateModel, neutralFactor)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- neutralFactor (str) – default neutral factor value for bend relief
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetOffsetRadius¶
-
PartSheetmetal.
SetOffsetRadius
¶ THE offset radius
Signature
SetOffsetRadius(updateModel, offsetRadius)
Parameters: - updateModel (bool) – Specifies whether the solid model be updated immediately
- offsetRadius (str) – default offset radius for joggle
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
SetOuterCornerTreatmentType¶
-
PartSheetmetal.
SetOuterCornerTreatmentType
¶ SETS the outer corner treatment type in Flat as Solid operation
Signature
SetOuterCornerTreatmentType(updateModel, outerCornerTreatmentType)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- outerCornerTreatmentType (
NXOpen.Features.SheetMetal.FeatureProperty
) – outer corner treatment type
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetOuterCornerTreatmentValue¶
-
PartSheetmetal.
SetOuterCornerTreatmentValue
¶ THE outer corner treatment value for Flat as Solid operations
Signature
SetOuterCornerTreatmentValue(updateModel, outerCornerTreatment)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- outerCornerTreatment (str) – default value for out corner treatment
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetStationaryRadius¶
-
PartSheetmetal.
SetStationaryRadius
¶ THE stationary radius
Signature
SetStationaryRadius(updateModel, stationaryRadius)
Parameters: - updateModel (bool) – Specifies whether the solid model be updated immediately
- stationaryRadius (str) – default stationary radius for joggle
New in version NX11.0.0.
License requirements: adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
SetThickness¶
-
PartSheetmetal.
SetThickness
¶ THE thickness value string
Signature
SetThickness(updateModel, thickness)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- thickness (str) – default thickness value for NX Sheetmetal solids
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetTool¶
-
PartSheetmetal.
SetTool
¶ The tool standard
Signature
SetTool(updateModel, standardName)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- standardName (str) – The name of a tool from the material standards file
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)