PartSheetmetalFlatPatternCalloutOrientationType Enumeration

NXOpen.Preferences.PartSheetmetal.FlatPatternCalloutOrientationType is an alias for NXOpen.Preferences.PartSheetmetalFlatPatternCalloutOrientationType

class NXOpen.Preferences.PartSheetmetalFlatPatternCalloutOrientationType

Bases: object

This enum represents orientation types for the flat pattern callouts

Enum Members

Enum Member Enum Member Description
Leadered
Leadered
Aligned
Aligned
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.