PartSheetmetalFlatPatternObjectType Enumeration¶
NXOpen.Preferences.PartSheetmetal.FlatPatternObjectType is an alias for NXOpen.Preferences.PartSheetmetalFlatPatternObjectType
-
class
NXOpen.Preferences.
PartSheetmetalFlatPatternObjectType
¶ Bases:
object
The members of the following enumerated type are used to identify object types to the FlatPattern API.
These are not the usual NX object types; they are ordinary NX objects that are known to the flat pattern feature for the type of outline they provide to a bend region, joggle region, or lightening hole.
Enum Members
Enum Member Enum Member Description BendCenterLine DeprecatedBendUpCenterLine BendDownCenterLine BendTangentLine OuterMoldLine InnerMoldLine ExteriorCurves InteriorCurves DeprecatedInteriorCutoutCurves InteriorFeatureCurves StrikePoint LighteningHoleCenter JoggleLine AddedTopGeometry AddedBottomGeometry ToolMarker -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-